Asking about pragma memory section in GCC build 1620 in S32DS 3.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Asking about pragma memory section in GCC build 1620 in S32DS 3.3

Jump to solution
7,154 Views
namnguyenviet
NXP Employee
NXP Employee

Hello guys,

In NXP GCC build 1620 integrated in S32DS 3.3, is that pragma for memory section has already supported? If yes, then do we have a note in the release note for that update? My customer in concern whether it's supported in our NXP GCC, as it's required in AUTOSAR OS concept. 

Many thanks,

Nam

Tags (4)
1 Solution
7,034 Views
alexanderfedoto
NXP Employee
NXP Employee

According to release notes in compiler directory (see <>/S32DS.3.3/S32DS/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/releasenotes.pdf) - yes it is:

pastedImage_1.png

View solution in original post

3 Replies
6,357 Views
comsytec
NXP Employee
NXP Employee

In version of 9.2.0 #pragma GCC section text ".mcal_text" has no effect for functions like snprintf, vsnprintf ... (standard functions) despite there is custom implementation of them and there is no prototype include before using desired mapping

#define ETH_43_PFE_START_SEC_CODE
#include "Eth_43_PFE_MemMap.h"

extern int snprintf(char_t *str, size_t size, const char_t *pcocStr, ...);
extern int vsnprintf(char_t *str, size_t size, const char_t *pcocStr, va_list VarArg);

Only __attribute__ is solution. Perhaps this is a bug.

0 Kudos
Reply
6,351 Views
comsytec
NXP Employee
NXP Employee

For builtin functions need to add options like
-fno-builtin-memcpy 
-fno-builtin-memset 
-fno-builtin-memcmp 
-fno-builtin-memmove 
-fno-builtin-strcmp 
-fno-builtin-strcpy 
-fno-builtin-strncpy 
-fno-builtin-strlen 
-fno-builtin-abs 
-fno-builtin-snprintf 
-fno-builtin-vsnprintf 

and then the

#define ETH_43_PFE_START_SEC_CODE
#include "Eth_43_PFE_MemMap.h"

achieving desired effect

0 Kudos
Reply
7,035 Views
alexanderfedoto
NXP Employee
NXP Employee

According to release notes in compiler directory (see <>/S32DS.3.3/S32DS/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/releasenotes.pdf) - yes it is:

pastedImage_1.png