Asking about pragma memory section in GCC build 1620 in S32DS 3.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Asking about pragma memory section in GCC build 1620 in S32DS 3.3

ソリューションへジャンプ
3,656件の閲覧回数
namnguyenviet
NXP Employee
NXP Employee

Hello guys,

In NXP GCC build 1620 integrated in S32DS 3.3, is that pragma for memory section has already supported? If yes, then do we have a note in the release note for that update? My customer in concern whether it's supported in our NXP GCC, as it's required in AUTOSAR OS concept. 

Many thanks,

Nam

タグ(4)
1 解決策
3,536件の閲覧回数
alexanderfedoto
NXP Employee
NXP Employee

According to release notes in compiler directory (see <>/S32DS.3.3/S32DS/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/releasenotes.pdf) - yes it is:

pastedImage_1.png

元の投稿で解決策を見る

3 返答(返信)
2,859件の閲覧回数
comsytec
NXP Employee
NXP Employee

In version of 9.2.0 #pragma GCC section text ".mcal_text" has no effect for functions like snprintf, vsnprintf ... (standard functions) despite there is custom implementation of them and there is no prototype include before using desired mapping

#define ETH_43_PFE_START_SEC_CODE
#include "Eth_43_PFE_MemMap.h"

extern int snprintf(char_t *str, size_t size, const char_t *pcocStr, ...);
extern int vsnprintf(char_t *str, size_t size, const char_t *pcocStr, va_list VarArg);

Only __attribute__ is solution. Perhaps this is a bug.

0 件の賞賛
2,853件の閲覧回数
comsytec
NXP Employee
NXP Employee

For builtin functions need to add options like
-fno-builtin-memcpy 
-fno-builtin-memset 
-fno-builtin-memcmp 
-fno-builtin-memmove 
-fno-builtin-strcmp 
-fno-builtin-strcpy 
-fno-builtin-strncpy 
-fno-builtin-strlen 
-fno-builtin-abs 
-fno-builtin-snprintf 
-fno-builtin-vsnprintf 

and then the

#define ETH_43_PFE_START_SEC_CODE
#include "Eth_43_PFE_MemMap.h"

achieving desired effect

0 件の賞賛
3,537件の閲覧回数
alexanderfedoto
NXP Employee
NXP Employee

According to release notes in compiler directory (see <>/S32DS.3.3/S32DS/build_tools/gcc_b1620/gcc-6.3-arm32-eabi/releasenotes.pdf) - yes it is:

pastedImage_1.png