After reinstalling S32 Design Studio for Power Architecture Version 2.1, a problem occurred and it c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

After reinstalling S32 Design Studio for Power Architecture Version 2.1, a problem occurred and it c

323 次查看
a17640336
Junior Contributor III

Today, because the software function was abnormal, I reinstalled S32d. The installation steps were based on the steps in the installation file.

 

However, after I installed it, S32d could not be executed. It popped up "This application cannot be executed on your computer." If you want to find a version suitable for your computer, please contact the software publisher's window.

 

And a log file is generated in the configuration folder in the eclipse folder.

Its contents are as follows:

!SESSION 2025-06-18 09:52:47.328 -----------------------------------------------
eclipse.buildId=unknown
java.version=1.8.0_202
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=zh_TW
Command-line arguments:  -os win32 -ws win32 -arch x86
 
!ENTRY org.eclipse.osgi 4 0 2025-06-18 09:52:47.694
!MESSAGE Application error
!STACK 1
java.lang.IllegalStateException: Unable to acquire application service. Ensure that the org.eclipse.core.runtime bundle is resolved and started (see config.ini).
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:78)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:388)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:243)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:62)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:498)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:673)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:610)
at org.eclipse.equinox.launcher.Main.run(Main.java:1519)

 

标记 (1)
0 项奖励
回复
1 回复

292 次查看
carlos_o
NXP TechSupport
NXP TechSupport

Hi @a17640336 

Thanks for your question.

Could you please provide the OS you are using? and which version of it are you using?

Are you using the same installer you use the first time or are you using a new download of the installer? 

 

0 项奖励
回复