Hello, I'm using S32DS 3.5 in Ubuntu 20.04.
I'm encountering some problems with adding the extensions to build the system.
I need to install S32K3 Real Time Drivers and FS26 SBC Autosar to build my system,
but these are not visible in my environment.
I tried to add these packages by downloading the zip file from nxp site, then add the update sites manually in 'S32DS Extensions and Updates' window, but still they are not visible.
I have attached the log collected via terminal.
Would there be any solution to solve this issue?
<<< Terminal logs >>>
OpenJDK 64-Bit Server VM warning: Ignoring option UnsyncloadClass; support was removed in 11.0
SLF4J: Failed to load class "org.slf4j.impl.StaticLoggerBinder".
SLF4J: Defaulting to no-operation (NOP) logger implementation
SLF4J: See http://www.slf4j.org/codes.html#StaticLoggerBinder for further details.
8월 03, 2022 11:09:20 오전 com.nxp.swtools.common.ui.utils.swt.internal.SWTFactory loadFont
경고: Could not load font from '/home/joung/NXP/S32DS.3.5/mcu_data/resources/fonts/RobotoCondensed/RobotoCondensed-Regular.ttf'.Native load failed. Check the path.
WebKit wasn't able to find a WebVTT encoder. Subtitles handling will be degraded unless gst-plugins-bad is installed.
log4j:WARN No appenders could be found for logger (org.apache.http.client.protocol.RequestAddCookies).
log4j:WARN Please initialize the log4j system properly.
(process:5771): GLib-CRITICAL **: 11:09:24.406: Failed to set scheduler settings: Operation not permitted