About the demo of FlexCan existed in S32 Design Studio 2018.R1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About the demo of FlexCan existed in S32 Design Studio 2018.R1

ソリューションへジャンプ
1,831件の閲覧回数
frank_feng
Contributor II

Recently , I start to use the demo flexcan_s32v234 existed in S32 Design Studio 2018.R1 , the demo is show below .

However when I debug this demo , I found the receive function works fine ,but the send function seems not working , I wonder before testing the send function of this demo if there is any configurations I need to change .According to my test, there is no output signal from pin A10 ,and if the demo works fine , there should be some output signal to be detected.Any information about this is needed , hope someone could give me some advice . I'll be very thankful 

the tool I used to get and send the frame message

111.PNG

the pin I used for my device is A10 and B10 

111.PNG

the send function which  is not working normal is show below

111.PNG

the demo I used is show below

111.PNG

0 件の賞賛
返信
1 解決策
1,772件の閲覧回数
frank_feng
Contributor II

it turns out the configuration of the dataInfo is not rightly set,after I change the setting of the dadaInfo as below shows ,sending function became normal

111.PNG

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,772件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi Cunjin,

Thanks for sharing the solution on community.

Stan

0 件の賞賛
返信
1,773件の閲覧回数
frank_feng
Contributor II

it turns out the configuration of the dataInfo is not rightly set,after I change the setting of the dadaInfo as below shows ,sending function became normal

111.PNG

0 件の賞賛
返信