About the demo of FlexCan existed in S32 Design Studio 2018.R1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the demo of FlexCan existed in S32 Design Studio 2018.R1

Jump to solution
1,813 Views
frank_feng
Contributor II

Recently , I start to use the demo flexcan_s32v234 existed in S32 Design Studio 2018.R1 , the demo is show below .

However when I debug this demo , I found the receive function works fine ,but the send function seems not working , I wonder before testing the send function of this demo if there is any configurations I need to change .According to my test, there is no output signal from pin A10 ,and if the demo works fine , there should be some output signal to be detected.Any information about this is needed , hope someone could give me some advice . I'll be very thankful 

the tool I used to get and send the frame message

111.PNG

the pin I used for my device is A10 and B10 

111.PNG

the send function which  is not working normal is show below

111.PNG

the demo I used is show below

111.PNG

0 Kudos
Reply
1 Solution
1,754 Views
frank_feng
Contributor II

it turns out the configuration of the dataInfo is not rightly set,after I change the setting of the dadaInfo as below shows ,sending function became normal

111.PNG

View solution in original post

0 Kudos
Reply
2 Replies
1,754 Views
stanish
NXP Employee
NXP Employee

Hi Cunjin,

Thanks for sharing the solution on community.

Stan

0 Kudos
Reply
1,755 Views
frank_feng
Contributor II

it turns out the configuration of the dataInfo is not rightly set,after I change the setting of the dadaInfo as below shows ,sending function became normal

111.PNG

0 Kudos
Reply