About the Max instruction in S32R274 SPT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About the Max instruction in S32R274 SPT

517 次查看
q_zhang
Contributor I

Hello ,

When I compile The Max instruction in S32DSv2.1, IDE reported an Error.

Max instruction:

maxs.ind .log2 .no_pre .thld_cmp .no_tag_in .tagged_vect .no_cyc_ext .in_24real .no_maxsn 32 WR_3, 256, 256, WR_47

Error:

maxs.ind .log2 .no_pre .thld_cmp .no_tag_in .tagged_vect .no_cyc_ext .in_24real .no_maxsn 32 WR_3,256,256,WR_47:  No version of instruction maxs matched the given arguments.

0 项奖励
1 回复

457 次查看
q_zhang
Contributor I

I find the src_add_inc  and the dest_add_inc in Max instruction can’t exceed 128

How can I implement the following instruction?

maxs.ind .log2 .no_pre .thld_cmp .no_tag_in .tagged_vect .no_cyc_ext .in_24real .no_maxsn 32 WR_3, 256, 256, WR_47

Thanks

0 项奖励