ADD PROCESSOR EXPERT

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ADD PROCESSOR EXPERT

跳至解决方案
2,317 次查看
linkeryip
Contributor I

Hello,

I am learning the S32 Desing Studio for the S32K144, when I am using the example code "MTRDEVKSPNK144_S32DS" kit, I can find and open a Processor Expert setting in the project.

Bun when I want to creat a new project myself, I can't create or add a new Processor Expert project to my SD32 Application Project. I search the help content, it imply I can creat the Processor Expert project with New->Others menu, but I can't find a Processor Expert option under this menu.

How can I start a Proecssor Expert project for my brand new SD32 application project?

Thanks in advance!

Best Regards,

Linker Ye

标记 (3)
0 项奖励
回复
1 解答
2,109 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复
1 回复
2,110 次查看
BlackNight
NXP Employee
NXP Employee

You have to select the correct SDK, see Tutorial: FreeRTOS 10.0.1 with NXP S32 Design Studio 2018.R1 | MCU on Eclipse 

I hope this helps,

Erich

0 项奖励
回复