S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
This document details how to create a new project in S32 Design Studio and build using the existing code and makefile provided within the NXP Vision SDK example projects. If you are creating a new makefile project with code from any other source, the procedure may be different. Before creating a new makefile project from existing code we need to add some paths to the environment variable PATH and a couple of new environment variables. There are 3 main methods for adding these paths and variables. Which method depends upon your needs. Method 1 The paths and variables can be added to each project individually. This is useful if you only want these changes to affect a small number of projects. Or if your projects require different paths and variables. Note: these changes would be made after the project is created (shown in steps 15 - 17 below) Method 2 The paths and variables can be added to the entire workspace within S32DS . These will not be visible outside of S32DS and therefore will not affect the entire Windows environment. This is useful if you have a large number of projects with common requirements for paths and variables and do not want them visible any tools outside of S32DS. Method 3 The paths and variables can be added globally to the Windows environment and will affect all installed tools. This method is not recommended. Once you have selected a method, add the following paths to the PATH variable (paths shown using the default installation settings for S32DS): C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm32-eabi\bin C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm64-eabi\bin C:\NXP\S32DS.3.1\S32DS\build_tools\gcc-6.3-arm64-linux\bin C:\NXP\S32DS.3.1\S32DS\build_tools\msys32\mingw32\bin or if within Eclipse (can use variables, which don't need to be updated should the layout of S32DS installation change in a future release) ${S32DS_ARM32_TOOLCHAIN_DIR} ${S32DS_ARM64_LINUX_TOOLCHAIN_DIR} ${S32DS_ARM64_TOOLCHAIN_DIR} ${S32DS_GCC_TOOCHAIN_DIR} It is also necessary to add the following Windows system variables: Variable Name: S32V234_SDK_ROOT Variable Value: C:\NXP\S32DS_Vision_v2018.R1\S32DS\s32v234_sdk Variable Name: APU_TOOLS Variable Value: C:\NXP\S32DS_Vision_v2018.R1\S32DS\APUC The following steps demonstrate the procedure based on Method 1 above. 1) Launch S32DS for Vision 2) Click New 3) Select 'Makefile Project with Existing Code' 4) Select Next 5) Enter a name for the project. 6) For 'Existing Code Location',    a) Select 'Browse...' and then select the directory  C:\NXP\S32DS.3.1\S32DS\software\VSDK_S32V2_RTM_1_3_0\s32v234_sdk\demos\isp\isp_sonyimx224_rgb_yuv_gs8    b) Click OK 7) For 'Toolchain for Indexer Settings', select the option which matches your desired build configuration. For our example here, we will select 'ARM Linux 64-bit Target Binary Toolchain'. See the Vision Extension Package User Guide for more details on the toolchain options. This sets up some toolchain paths, but later we will set more for the specific needs of the VSDK examples. 😎 Click Finish 9) Right-click on the project from the Project Explorer. Select Properties 10) Go to section 'C/C++ Build' 11) Go to the 'Behavior' tab and in the field next to 'Build', enter:    ISP examples: 'allsub'    APEX examples: 'APU_COMP=nxp allsub' 12) Go to 'Builder Settings' tab, in 'Build location' section change the path for the 'Build directory'. Click on 'Workspace...' button 13) In the Folder selection menu, select the subfolder 'build-v234ce-gnu-linux-d' and click OK 14) Go to section 'Environment' 15) Select the environment variable 'PATH' and click 'Edit...' 16) Add the path variables to the value field, each separated by a comma ';' ${S32DS_ARM32_TOOLCHAIN_DIR} ${S32DS_ARM64_LINUX_TOOLCHAIN_DIR} ${S32DS_ARM64_TOOLCHAIN_DIR} ${S32DS_GCC_TOOCHAIN_DIR} Click OK 17) Click 'Add...' 18) Click 'Add...' and enter variable name 'APU_TOOLS' and value '${S32DS_APU_TOOLCHAIN_DIR}' Click OK 19) Click OK to close the Properties menu. 20) Click on 'Build' 21) Once the build is complete, the binary file (ELF) will be created
查看全文
In this document, we show the steps to use the New Project Wizard to create a new application project for APEX2, ISP, or both.   1. Launch S32DS for Vision 2. Select File -> New -> S32DS Application Project 3. Enter a name for the project 4. Select the 'A53 APEX2/ISP Linux' processor option 5. Click Next 6. Select the APEX2/ISP options you need.       a. APEX2 programming - will add support to your project for an APEX2 application, you need this for any new APEX2 project       b. ISP programming - will add support to your project for an ISP application, you need this for any new ISP project       c. ISP visual modeling - will create a separate project for your ISP data flow diagram, you will not need this if you plan to use an existing graph diagram. This can also be created later. 7. Select the SDK(s) as appropriate for your setup. For example, 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS, the one which corresponds to your OS is selected for you by default. 7. Click Finish 8. You now have a project or set of projects for development on the S32V234.
查看全文
One of the many great features of the S32DS is the ability to access the Linux BSP file system on the SD card in the S32V234-EVB. Once connected, you can drag and drop files between your PC and the EVB. Once you have completed HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP  and HOWTO: Setup A Remote Linux Connection in S32DS (S32V234), you are ready to setup the Remote Systems view to connect to the Linux files system to view and access the file system. Prerequisite Before starting this procedure, make sure the BSP is loaded onto the SD Card, the SD Card is inserted into the SD Card Slot, the ethernet cable is connected to both the EVB and the network port, and the EVB is powered up. 1) Go to 'Window -> Show View -> Other' 2) Expand 'Remote Systems', then select "Remote Systems' and click OK 3) Click 'Define a connection to remote system' button OR right-click in the Remote Systems window and select 'New Connection...' from the list Right-click menu 4) Select 'SSH Only' 5) Enter the IP address noted from HOWTO: Setup A Remote Linux Connection in S32DS (S32V234) for Host name, enter a descriptive name for the connection (optional) and click Finish. 6) Right-click on the connection name in the Remote Systems window and select 'Connect' OR expand the folders under the connection name until the login window appears: Connection_name -> Sftp Files -> Root (window appears) 7) Enter "root" for User ID and since the BSP comes with ID root without a set password, leave the password field blank. 😎 Click OK 9) The Linux file system is now visible in the Remote Systems window. You can drag and drop files to and from here. Expand the folders to see the contents.
查看全文
The Vision SDK root is contributed to the Design Studio as a dynamic path variable “S32DS_VSDK_DIR”. Several Design Studio services use this variable to access the resources inside the Vision SDK. By default, this variable points to “${eclipse_home}../S32DS/s32v234_sdk”, i.e. to the Vision SDK shipment bundled with Design Studio. Technically you can change this variable to point to another instance of Vision SDK using the following steps: 1. Go to the main menu "Window -> Preferences" 2. Filter the preference dialog with "sub" keyword or just navigate to "Run/Debug -> String Substitution node. 3. Edit Variable "S32DS_VSDK_DIR" to assign another value to be substituted as Vision SDK root 4. Press OK when changes are complete.
查看全文
There are a number of existing ISP Graph diagrams provided within the VSDK. It is possible to import them into S32DS and use them in a new C/C++ project. The steps to do this are detailed within this document. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select File -> New -> S32DS Application Project. 3) Enter a project name, such as: ISP_ISP_Generic_demo 4) Select 'A53 APEX/ISP Linux' 5) Click Next 6) Deselect the APEX2 options and 'ISP Visual Modeling' option. 7) Click Finish 😎 Select File -> New -> S32DS Project from Example. 9) Select isp_generic. 10) Select Finish 11) Open isp_generic in the project explorer 12) Double-click ISP data flow ; isp_generic. The ISP data flow graph will appear in the editor 13) Define a new configuration for emitting code from the graph       a) Right-click in the ISP data flow window and select Emit As -> Emit Configurations...       b) Select ISP Emitter       c) Press New Launch Configuration       d) Enter a name       e) To select the graph, press Browse Workspace       f) Expand each item until you can select the .isp file. Click OK       g) Select the location of the emitted output to the application project, select Browse Workspace       h) Select the name of your application project, then press OK       i) Enter 'A53_gen' to the Dynamic sequences sources folder box. This is the folder within the target project that generated code will be stored. Check the box for Emit host code.       j)Now select the location to store the configuration file. Go to the Common tab, select Shared file and click Browse       k) Select the .launches folder inside ISP_ISP_Generic_demo and click OK       l) Click Apply and Emit. Dialog box will appear when code generation is successful              m) Expand the folders within ISP_ISP_Generic_demo, A53_gen, src and inc, to see the newly generated output files 14) Build the project 'ISP_ISP_Generic_demo' for ISP 15) Open file 'ISP_ISP_Generic_demo/A53_inc/isp_user_define.h', by double clicking on it in the Project Explorer. Change '#define DCU_BPP DCU_BPP_YCbCr422' to '#define DCU_BPP DCU_BPP_24' and change '#define __DCU_BPP' to "#undef __DCU_BPP". Before After 16) Using the method detailed in steps 8 - 10, create the example project 'isp_sonyimx224_csi_dcu'. Take from this project the file 'isp_sonyimx224_csi_dcu/A53_src/main.cpp' and use it to replace the file 'ISP_ISP_Generic_demo/A53_src/main.cpp' in the current project. Then make the following modifications:  On line 36, change <#include "mipi_simple_c.h"> to <#include "isp_generic_c.h">. On line 303, change <gpGraph_mipi_simple> to <gpGraph> AND <gGraphMetadata_mipi_simple> to <gGraphMetadata> On line 330, change <FDMA_IX_FastDMA_Out_MIPI_SIMPLE> to <FDMA_IX_ISP_OUTPUT>. Please see C:\NXP\S32DS.3.1\S32DS\software\VSDK_S32V2_RTM_1_3_0\s32v234_sdk\docs\drivers\SDI_Software_User_Guide.pdf for details on what this code is for. 17) In Project Explorer, right-click on "...\A53_gen\src\isp_process.cpp" and select Build path -> Remove from -> A53 18) Select 'ISP_ISP_Generic_demo:A53' in the Project Explorer panel, then Build for A53 19) Run it remotely on the target using the method fromHOWTO: Create S32V234 Cortex-A53 Linux Project in S32DS . Should get results similar to this:
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 9          What is new? S32K1xx SDK RTM 3.0.0 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148  (S32K1xx SDK release notes) AMMCLIB version 1.1.15  (AMMCLIB S32K14x release notes) Segger J-Link drivers v6.42a (J-Link release notes) This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6, Update 7, Update 8) Installation instructions The update is available for online (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided ISP examples through to execution on the EVB is detailed. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select "New S32DS Project from example" 3) Select isp_sonyimx224_csi_dcu project and click Finish.    In this particular project, the ISP graph diagram is included. If you wish to view it, go to the Project Explorer panel and expand 'isp_sonyimx224_csi_dcu_graph'. Then double click on 'ISP data flow : mipi_simple'. The ISP graph diagram will appear in the editor panel. 5) We are ready to build the project, but first, select isp_sonyimx224_csi_dcu: A53 in the Project Explorer panel 6) Build project for A53  7) Start a debug session using method as described in HOWTO: Create S32V234 Cortex-A53 Linux Project in S32DS, beginning at step 10. 😎 Should get results similar to this:
查看全文
This tutorial walks a user through the steps to create a new application for the S32V234 MCU using S32DS (with S32V2xx development package and Vision extension package for S32V2xx) and the built in APEX2 Visual Graph tool. The completed application will take a PNG image, upscale and downscale it using APEX engines and return the processed images. Prerequisites: Some knowledge of the S32V234 System on a Chip (SoC) Have an understanding of the APEX architecture and APEX Core Framework (ACF) Refer to UG-10267-03-14-ACF_User_Guide.pdf to learn about ACF Path: s32ds_install_dir\S32DS\software\VSDK_S32V2_RTM_x_x_x\s32v234_sdk\docs\apex\acf Be familiar with the NXP Vision SDK software Looking for Interactive Tutorial? You can view this tutorial as a video, go to Getting started with S32 Design Studio IDE including Vision Extension Package for S32V processors | NXP and select '4 | Create a new APEX2 application'
查看全文
This tutorial walks a user through the steps to create a new application for the S32V234 MCU using S32DS (with S32V2xx development package and Vision extension package for S32V2xx) and the built in ISP Visual Graph tool. The completed application will take an image from camera, processes it on ISP and put the processed image in DDR buffers. Once the image is in DDR buffer, host (A53 core running Linux) will direct the display control unit (DCU) to display it on screen. Prerequisites: Some knowledge of the S32V234 System on a Chip (SoC) Have an understanding of the ISP architecture Be familiar with the NXP Vision SDK software Looking for Interactive Tutorial? You can view this tutorial as a video, go to Getting started with S32 Design Studio IDE including Vision Extension Package for S32V processors | NXP and select '3 | Create a new ISP Application'
查看全文
Getting started with APEX2 S32DS: Getting Started - APEX2 Graph Tool Tutorial  Getting started with ISP S32DS: Getting Started - ISP Graph Tool Tutorial 
查看全文
So you have created a project in S32DS with target of S32V234 Cortex-A53 APEX2/ISP Linux . You have built the project and now want to execute it on the S32V234-EVB2, which is running the Linux BSP for the VSDK on a microSD card. There are many ways to do this, however, the simplest is to use the built-in support within S32DS to run and/or debug over an Ethernet connection to the Linux BSP OS running on the EVB. In order for S32DS to connect to the Linux BSP OS, the following steps should be followed: 1) First, we must complete the steps in HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP . 2) With the Linux running on the EVB, start a terminal program (for ex. PuTTY) on your PC 3) Set Connection type to Serial 4) Set speed to 115200, Data bits 8, Stop bits 1, Parity None 5) Set Serial line to the COM port associated with the USB port setup in step 1 of this document. (for ex. COM3) 6) Click Open to start the terminal session 7) Press enter key to bring up login prompt 😎 Log into Linux (login name is "root") 9) Get IP address, enter command:    ifconfig       Make note of the IP address 10) Launch S32DS for Vision. From the C/C++ Perspective, select Run->Debug Configurations... 11) From 'C/C++ Remote Application'. Select '<project_name>_Remote_Linux' debug configuration. 12) Select New to create new debug connection. 13) Select SSH 14) Enter the IP address noted earlier 15) Enter user ID as "root". The Linux BSP uses Password based authentication, but by default, no password is set. So the password can be left blank. 16) Select Finish 17) Select Apply, and then if you wish, Debug This connection is stored within the workspace. It can be added to any projects within the workspace. If a new workspace is created, then this connection will not appear in the selection list.
查看全文
While the S32V234-EVB2 comes shipped with an SD card preloaded with a Linux Board Support Package(BSP), it does not support the Vision Software Development Kit(VSDK). This you will have to load yourself. There are two methods for installing the S32V234 BSP for VSDK to your SD card: 1) Download the image file from your Software Account on nxp.com and write the file to the SD card, or 2) Create the image on the SD card from ubuntu installed on a PC or virtual machine Download the image file and write it to SD card This is the simplest method, but does not allow for much customization. It is an excellent choice for those users who do not have much experience with Linux or just need something quick to get up and running with S32 Design Studio, try out the application examples, etc. Procedure 1) Login to your account on NXP.COM (if you do not already have an account, then just register for one) 2) Go to Vision SDK Software  3) Accept the license agreement 4) Select the version of VSDK you wish to use 5) Check the box next to 'VisionSDK RTM x.x.x pre-built SD Card image based on Yocto rootfs' and click 'Download selected files'. This will download the .gz file to your PC. 6) Unpack the VisionSDK_S32V2_RTM_x_x_x_img_yocto.tar.gz archive file 7) Unpack the VisionSDK_S32V2_RTM_x_x_x_img_yocto.tar archive file 😎 Navigate to the '\build_content\v234_linux_build\s32v234evb' folder, then unpack the sdcard-evb.tar.bz2 file 9) Unpack the sdcard-evb.tar file 10) The resulting file is sdcard-evb.img. You can use an image writing tool (such as Win32 Disk Imager download | SourceForge.net) to write this image file to the SD card. You will need to use the SD card adapter to insert the microSD card into the SD card slot on your PC, if available. If you do not have an SD card slot on your PC, there are many SD card-to-USB adapters available on the market. 11) The SD card is now ready to inserted into the SD card slot on the S32V234-EVB2 SD card slot. Create the image on SD card from ubuntu This is a better choice for more advanced users who wish to customize the BSP. To prepare an SD card for a Linux boot, it is necessary to connect the SD card to a machine with Linux OS. If a Linux OS machine is not available, then a virtual machine installed to a Windows OS machine may be used. If you have access to a Linux OS machine, skip to step 4. Procedure 1) Download and install a virtual machine VMware Workstation Player Virtual Box 2) Download Ubuntu. This tutorial uses the Ubuntu version 14.04.5.  The image will be ubuntu-14.04.5-desktop-amd64.iso. 3) Launch VMware or Virtual Box and create a new virtual machine Use downloaded Ubuntu image when requested for installer disc image file Hit Next and select Linux as the guest operating system and select Ubuntu for the version. Hit Next and name your virtual machine and specify where you want to store it. Increase the disk size to 40 GB Hit Finish and install VMware Tools for Linux, if asked 4) Within C:\NXP\S32DS_Vision_v2.0\S32DS\s32v234_sdk\os extract 'build_content.tar.gz', then extract 'build_content.tar' and navigate to the 'v234_linux_build' folder 5) Start virtual machine May need to manually connect USB-mounted SD card reader Log in to virtual machine 6) In files, go to 'Home' directory and create a folder "VSDK" 7) Within VSDK folder, copy the files image, u-boot.s32, s32v234-evb.dtb, and rootfs.tar from the 'v234_linux_build' folder.  Note: The file s32v234-evb.dtb and u-boot.s32 will have names with XXXXX-suffix for the schematic number printed on the evaluation board (EVB) you are using. Be sure to use the files which correspond to your EVB. 😎 Load the card into the reader. If you are using a virtual machine, it is recommended to use a USB adapter instead of a built-in reader in the PC. 9) Within the virtual machine, launch the terminal program 10) Within the terminal program, enter command 'cat /proc/partitions' to view the names of the partitions and identify the names of the partitions on your SD card. Perhaps it is named 'sdb'. 11) Delete all existing partitions.    a) Enter command 'sudo fdisk /dev/sdb'.    b) Enter command 'd' and then the number of the partition to delete. Repeat as necessary until all partitions have been deleted 12) Create new partitions    a) Enter command 'n' for new    b) Enter 'p' (or just hit <enter>, as this is the default) for primary    c) Enter '1' (or just hit <enter>, as this is the default) for partition number 1.    d) Press <enter> to select the default value for the First sector    e) Enter '+255M' to set the size    f) Enter command 'n' again, for partition number 2, however, press <enter> to select the default value for the 'Last sector' 13) Set the partition type    a) Enter command 't' for type    b) Enter '1' for partition number 1    c) Enter 'c' for partition type FAT32    d) Enter command 't' again, for partition number 2, however, enter '83' for partition type LINUX If you get error 16: Device or resource busy, as shown above, use commands 'umount /dev/sdb1' and 'umount /dev/sdb2' to free the pre-existing partitions. Then try again and should be ok now 14) Write the new configuration, enter 'w' 15) Try to setup the filesystems. Enter 'sudo mkfs.vfat -n boot /dev/sdb1'. If you get the error '/dev/sdb1 contains a mounted filesystem', you will need to unmount the partition first. To save time, unmount both /dev/sdb1 and /dev/sdb2. Enter 'umount /dev/sdb1' and then 'umount /dev/sdb2' Now try 'sudo mkfs.vfat -n boot /dev/sdb1' again 16) It worked, so now enter 'sudo mkfs.ext3 -L rootfs /dev/sdb2'. It will take a minute or two for this to complete. Wait until you get the command prompt again. 17) Now it's time to load the BSP content from the VSDK. But first, change the directory to the one we created earlier for the BSP files. Enter 'cd /home/user/VSDK' or 'cd VSDK'. Enter the following commands: sudo dd if=u-boot.s32 of=/dev/sdb bs=512 seek=8 conv=fsync sudo cp Image /media/user/boot sudo cp s32v234-evb.dtb /media/user/boot 18) Now we need to extract the root filesystem, change the directory to its location 19) Enter command 'sudo tar -xvf /home/user/VSDK/rootfs.tar' 20) Once the files are extracted, enter command 'sync'   Now the SD card is ready to be used in the S32V234-EVB.
查看全文
Before you can start debugging an S32DS project for S32V234 Cortex-A53 APEX2/ISP Linux target on the S32V234-EVB2, we must first setup the hardware connections and start the Linux BSP OS. 1) Connect (1) S32V234 USB Micro B port to (2) USB A port on your PC. This allow you to connect to the Linux BSP OS via a terminal program to issue commands and to obtain the IP address. 2) Insert microSDHC card (with U-boot, Linux kernel, devicetree, and root file system loaded*) into (3) the S32V234 EVB2 microSD card slot   3) Connect (1) Ethernet port on S32V234 daughter card to (2) LAN**. This will allow S32DS to communicate with the Linux BSP OS for flashing and GDB debugging.   4) Connect the power supply to (3) S234V234 EVB 5) Turn on the (4) power switch, this will start the Linux BSP OS *Instructions for preparing the SD card are provided in the VisionSDK document: ..\S32DS.x.x\S32DS\software\VSDK_S32V2_RTM_x_x_x\s32v234_sdk\docs\vsdk\S32V234-EVB_SetupGuide.pdf or refer to HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB2 Using BSP For VisionSDK  **Ensure PC is connected to LAN as well (either hardwired or wireless)
查看全文
So you've just installed the S32DS and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started. Prerequisite Before following the steps in this HOWTO, ensure you have the S32V2xx development package installed to S32DS. 1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click the '...' next to the SDKs field 7. Check the box next to 'VSDK_MODULE_WIN' for Windows OS or 'VSDK_MODULE_LINUX' for Linux OS and click OK. 8. Click Finish 9. Build the project for Debug 10. Project is now built, ELF file is ready to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB2 for debugging with S32DS and Linux BSP. 11. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS (S32V234)  12. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 13. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 14. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 15. The executable file is copied to Linux file system and gdbserver starts. 16. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
查看全文
S32DS for Vision contains many example projects from which you can learn how S32DS, with the Vision Extension Package for V2xx, can be used with the help of the Vision SDK to develop vision applications. The example projects contain generated and hand-written code, which utilize the Vision SDK to demonstrate a workflow using S32DS. In this document, the procedure for creating a project from one of the provided APEX2 examples through to execution on the EVB is detailed. Prerequisite Before following the steps in this HOWTO, ensure you have the Vision Extension Package for V2xx (as well as the S32V2xx development package) installed to S32DS. 1) Launch S32DS 2) Select 'New S32DS Project from example' 3) Select apex2_fast9 project 4) Click Finish 5) Select apex2_fast9: A53 in the Project Explorer panel. Build the project using build config 'TEST_A53'. 6) Start a debug session using method as described in HOWTO: Create A53 Linux Project in S32DS for Vision, beginning at step 9. 7) Click Resume  Should see something similar to what is pictured below There are green diamonds at the corners in the image as identified by the fast9 corner detection algorithm
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio 2018.R1         Austin, Texas, USA December 28, 2018   The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio 2018.R1 for S32 Automotive Platform|NXP.  Major features  • NXP GCC toolchains for ARM32 and aarch64 bareboard and Linux targets  (GCC version 6.3.1 20170509, build 1574 revision g924fb68) • S32 Debug Probe support provided with S32 Debugger (support for S32V23x, RAM + FLASH) and S32 Trace tool for S32V23x • S32 Trace tool is integrated to provide software analysis features (profiling, code coverage, and other) • PEMicro® hardware debugger support provided with P&E Debugger • Lauterbach Trace32® support • S32 Flash Tool is delivered to support Flash/SD/MMC memory programming for S32V234 • S32 SDK for S32V23x 0.8.1 EAR is integrated • S32DS Extensions and Updates tool for automatic lookup and on-demand installation of software packages adding support for the NXP Arm® based processor families • S32 Configuration Tool framework (EAR6) with the Pin, Clock, Peripheral configuration tools Complete S32 Design Studio 2018.R1 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application package available is Vision S32V2xx  (Other packages are coming soon). The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
查看全文
This document shows, how to set optimization level for whole project and how to edit single files with different optimization level. As soon as the project is created, it has set optimization level to 0 by default. This means, compiler do neither size optimization nor speed optimization. Optimization level can be set for every project according to the project requirements. 1) Optimization level set Right click the project and select project properties. Click C/C++ Build ->Settings->Standard S32DS C Compiler ->Optimization. You can see, optimization level is none -O0. Click the arrow on the right side of the list and choose the required optimization level. There are five options you can choose. Details description of the options are included in S32DS reference manual. Chosen optimization is used for all files in the project. 2) Change optimization level for single file in the project If you want to change optimization level for single file and do no affect another files, select required file, right click on it and select properties. As you can see, there are limited possibilities to set the file itself. Select required optimization level, click apply and close the window. Now, selected file has different options than the rest of the project. Hope it helps. Martin
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 9          What is new? S32 SDK for Power Architecture 2.0.0 RTM supporting  MPC5741P, MPC5742P, MPC5743P, MPC5744P, MPC5744B, MPC5745B,  MPC5746B, MPC5744C, MPC5745C, MPC5746C, MPC5747C, MPC5748C, MPC5746G, MPC5747G, MPC5748G, S32R274, S32R372 (see the S32 SDK release notes) AMMCLIB version 1.1.14 (see the AMMCLIB MPC574xP example release notes) Radar SDK RTM, version 1.2.0 (see the RSDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8 ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
1. Modify your application to be compatible with RAppID BL tool. Add memory space for delay and application key in linker file (modified hello world project is in attachment):   Add data for this sections in your app (for example in main.c file): 2. Flash MPC5744P.rbf file into MCU. You can create new empty project or use existing one. Start debug Configurations and Browse MPC5744P.rbf file (located in [YOUR_RAPPID_INSTALL_FOLDER]\RBF_Files. Start debug session.  3. Modify your EVB - add jumper wire from J3-4 to J2-16  and J3-2 to J2-14. RAppID uses UART0 and to USB is connected UART1.   4. Start RAppID BL tool, select COM port where EVB is connected,  choose your s-record file and Start Boot Loader:
查看全文
This document describes, how to add software site and how to install update from the 3rd party software site. 1) In S32DS, click Help->Install New Software 2) Click Available Software Sites. 3) Select required site, if available. 4) Select required site in Work with line: 5) Available updates will appear in the window below. Check GNU E200 PEMicro Interface Debugging Support 6) Click Next and new window will appear. Select required software and click Next. 7) Accept the license terms and click Finish. New software will be downloaded and installed. Hope it helps. Martin
查看全文