S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
This document details the steps to program external EEPROM with the 32 reset configuration bits in support of the 'Boot from serial RCON' method detailed in the S32G Reference Manual. The Python scripts used for this task are designed and tested to work on the S32G-VNP-EVB with S32G2xx Rev2 and the Atmel AT24C01C it contains.(Serial EEPROM is not implemented on NXP VNP-RDB board)   The RCON can be set by the following: Fuses (internal to the device) Parallel (GPIO pins/DIP Switches on EVB) Serial (EEPROM connected via I2C) The Serial option can be programmed using a debug probe connected via JTAG. This enables the RCON to be controlled remotely, assuming the debug probe is setup to allow remote connections.    Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. This is important as the S32 Debugger provides access to the EEPROM programming capabilities via I2C of the S32 Debug Probe.  Connect the S32 Debug Probe to the S32G-VNP-EVB and the host PC containing S32 Design Studio installation. Set BOOTMOD pins to boot from RCON Set BOOT_CFG[8]=1 on the S32G-VNP-EVB, for serial RCON mode VNP-EVB shown here with switch BOOT_CFG[8] = 0 See the EVB documentation and device reference manual for more details. Procedure   Open cmd window to the S32 Debugger folder where the device-specific scripts are located. C:\NXP\S32DS.3.4\S32DS\tools\S32Debugger\Debugger\scripts\s32g2xx Set Python path so correct version is used (if not already set in env vars) set PYTHONPATH=C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7;C:\NXP\S32DS.3.4\S32DS\build_tools\msys32\mingw32\lib\python2.7\site-packages Edit the python script to adjust the value to be programmed to RCON, s32g2xx_i2c_RCON.py. Note: The listed examples show only the minimum values required to configure each of the external memory types. Additional settings may be required for your specific application. Adjust the RCON_DATA for the configuration you wish to program.  Do not adjust RCON_ADDR. Adjust the S32DBG_IP for the IP address of your S32 Debug Probe.  Adjust the INTERACTIVE_MODE  Set True, if desired to be prompted to enter RCON_DATA Set False, if desired to have script automatically enter RCON_DATA, based on the value set within the file. Adjust _SOC_NAME as appropriate for the specific S32G2xx device you are using. The valid options are defined in s32g2xx_context.py. Enter the command to start GDB, passing in the RCON Python script: Windows OS: C:\NXP\S32DS.3.4\S32DS\build_tools\gcc_b1620\gcc-6.3-arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32g2xx_i2c_RCON.py OR C:\NXP\S32DS.3.4\S32DS\build_tools\gcc_v9.2\gcc-9.2-arm32-eabi\bin\arm-none-eabi-gdb-py.exe -x s32g2xx_i2c_RCON.py Linux OS: arm-none-eabi-gdb-py -x .\s32g274a_i2c_RCON.py If everything worked properly, then the value you programmed will be displayed to the screen. To exit GDB, enter 'quit'.
查看全文
1) Prepare the evaluation board hardware You can use the S32 Debug Probe to download code to target Connect S32 Debug Probe to S32V234 EVB using JTAG connector Connect S32 Debug Probe to PC via USB cable OR ethernet (if connected via ethernet, then USB power cable must also be connected) Connect the S32V234 EVB to PC via ethernet (typically via LAN) Connect power cable to evaluation board and switch on the power     2) Build the project using the A53 build option. 3) Start debug on A53 core. Project is now built, ELF file is read to be loaded to EVB for execution. 4) Before a debug session can be started, we must complete HOWTO: Setup A Remote Linux Connection in S32DS for Vision. 5) Select the debug drop-down menu and click Debug Configurations     6) Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 4 is selected (points to the IP address of your EVB). Click Debug     7) The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed.     The executable file is copied to Linux file system and gdbserver starts.   You may get an error message on the first try, this is normal. Just try it again and it will work. 😎 Once the Linux GDB has started on A53 core and the initial break point is reached in main(), it is almost ready for to start debug on ISP. Click Resume as the A53 must be running before we can attach the ISP debug thread. 9) Locate the ISP debug configuration from the Debug Configurations menu. You will see a debug configuration within the 'S32 Debugger' group (in our example, isp_sonyimx224_csi_dcu_ISP as shown below). This is the debug configuration we will use, however, it will require some setup.     10) You should notice the error message at the top of the window, just below the title and a red 'X' on the Debugger tab. Click on the Debugger tab to select it. We must setup the Debug Probe Connection before we can proceed. There are two options: Ethernet USB   If connecting the Probe via Ethernet, please refer to the Quick Start Guide or S32 Debug Probe User Guide provided with the S32 Debug Probe for instructions on how to connect it and determine the Hostname or IP address.     If connecting the Probe via USB, then the COM port will appear in the Port selection setting. If you have more than one S32 Debug Probe connected, you will need to determine which COM port is the correct one, otherwise, only the COM port for your S32 Debug Probe will appear.   11) This is already done for our example, but for your application, it may be necessary to setup the symbols for the ISP engine. Go to the Startup tab and:    a) Check the box for 'Load symbols'    b) Select the option for 'Use file', click Workspace... and locate the object file (.opius) for the ISP engine you wish to debug.   12) Click Apply then Debug. It may take a few moments for the APEX core debug to launch.   13) Wait for the ISP debug launch to complete. You may notice the A53 thread has terminated. This is normal and expected since the camera input cannot be suspended. When the launch completes, the context of the Debug window will switch to the ISP debug thread. 14) Enable Instruction Stepping mode and then step one time to load the object file which was setup in step 6. 15) The ISP debugging is now running and you can step through the ISP engine, look at registers, set a break point, etc. Note: only one hardware break point is supported for ISP.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 9          What is new? S32 SDK for Power Architecture 2.0.0 RTM supporting  MPC5741P, MPC5742P, MPC5743P, MPC5744P, MPC5744B, MPC5745B,  MPC5746B, MPC5744C, MPC5745C, MPC5746C, MPC5747C, MPC5748C, MPC5746G, MPC5747G, MPC5748G, S32R274, S32R372 (see the S32 SDK release notes) AMMCLIB version 1.1.14 (see the AMMCLIB MPC574xP example release notes) Radar SDK RTM, version 1.2.0 (see the RSDK release notes) This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7, Update 8 ). Installation instructions The update is available for online installation (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
Introduction In this document, we will discuss the S32DS Extensions & Updates tool and how to use it to install the device support you need.   S32 Design Studio for S32 Platform has been designed to allow users to customize their installation, enabling them to integrate support for just the NXP devices they need and just the tools they need. With the new modular design, parts of the tool have been moved into one of 4 different package types. The Platform and Tools Packages are default packages which are included as part of the base install, cannot be uninstalled, however, they can be updated.   The Platform package contains the base components of the IDE, modular installer, general documentation and integration mechanisms. The Tools Package contains the compilers, debuggers, and MSYS2. The Development Package contains hardware specific support such as New Project Wizard, S32 Configuration Tools, SDKs and Libraries. The Extension Package contains Accelerator Compiler, Debugger, Graph Tool and advanced SDKs.   Downloading the various components from our cloud-based update server, allows you to assemble and complete the customized installation of the tools and software to meet your development needs. It is also via the update server that the updates and bug fixes will be provided. And of course, all of these will be available as downloads from our product page for users who are installing to an offline PC. S32DS Extensions and Updates Menu When you first launch the S32 Design Studio for S32 Platform, you are presented with the S32DS Extensions and Updates menu. This menu provides a listing of the add-on packages which have been installed, those that are available to be installed, and those which have updates available to be installed. In the panel to the right is displayed detailed information specific to the package which is selected in the panel to the left. If there is an update available for the selected package, the currently installed version number will be shown on the left and the update version number will be shown on the right.       Online Package Installation Setup If your PC is connected to the internet, then it will link to NXP's update server (http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_3.5) and any new or updated packages will be automatically added to the list. See Package Installation section below for installation procedure and details.       Offline Package Installation Setup If your PC is not connected to the internet, you must first download the desired packages from the NXP website, in the form of an archive file, to a separate PC and have them transferred to your target PC. Then you would select the link 'Go to Preferences' and add each downloaded archive file as a separate software site. After selecting OK, you will see the new packages contained within the archive files listed.   Procedure: Go to S32 Design Studio for S32 Platformdownload page and select Download for the package or update you need. Once the file is downloaded, it must be installed within S32 Design Studio. Launch S32DS and wait for the S32DS Extensions and Updates window to appear. Then select the 'Manage Sites' link. The Preferences window appears. Select the 'Add...' button to add a new software site to the list. The file you downloaded will be a software site. Now the Add Site window appears. Since the downloaded file is an archive of type ZIP, the 'Archive...' button should be used to select it. Navigate to the location where the file was saved. Now the downloaded file has been added as a new site. Select OK to return to the main S32DS Extensions and Updates window. Now the new package(s) will appear in the S32DS Extensions and Updates window, just as it would from the update server. See Package Installation section below for installation procedure and details.   Package Installation To install the new packages or updates, check the box to the left of the desired package in the left panel and select 'Install/Update'. The tool will automatically detect any dependencies on other packages and select them to meet all requirements for the installation.     Follow the prompts and the packages will be installed, followed by a request to restart S32 Design Studio.     Dependencies and Errors If there are dependencies between two or more updates, the tool will detect this and inform you of the package which cannot yet be installed. If you try to install a package which is not compatible with the version of S32 Design Studio you have installed, a notice will appear, and the package will not be listed in the S32DS Extensions and Updates menu.   Uninstalling Unwanted Packages If you no longer need a particular package or installed one by mistake, just check the box next to the package and select 'Uninstall'.       Reinstalling Packages If you believe your installed package has become corrupted, if you accidentally deleted part of it (such as an example project, etc.), or if for any reason you need to restore the package, just check the box next to the package and select 'Reinstall'.   Additional Information If you wish to not see the S32DS Extensions and Updates menu at startup, you can uncheck the box at the lower left. For internet connected PCs, the update server will still be linked and checked for new packages at S32DS startup, but you will no longer see the S32DS Extensions and Updates menu. However, you will still see a notice at the lower right of the tool at startup when new packages are detected.      
查看全文
So you've just installed the S32DS for Vision and are using it for the first time and would like to see how it works. Here is a quick and simple project to get you started.   1. Launch S32DS for Vision 2. Select 'S32DS Application Project' 3. Enter a name for the project 4. Select the 'A53 Linux' processor option 5. Click Next 6. Click Finish 7. Change to C/C++ perspective, click on 'Switch to C/C++ Development' 8. Build the project for Debug 9. Project is now built, ELF file is read to be loaded to EVB for execution. However, if we have not prepared the EVB, we must first complete HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP. 10. Once the EVB is properly prepared, we must complete HOWTO: Setup A Remote Linux Connection in S32DS for Vision. 11. With the project debug configuration and remote linux connection selected, select the debug dropdown menu and click Debug Configurations 12. Make sure the Debug_Remote_Linux debug configuration is selected and the connection setup in step 10 is selected (points to the IP address of your EVB). Click Debug 13. The first time you connect to a new IP address (i.e. the first time you debug after booting the board), you will receive a warning message, Click Yes and proceed. 14. The executable file is copied to Linux file system and gdbserver starts. 15. The Debug perspective is opened. You can now step through the code*     *Only debugging of the A53 code is supported by Linux GDB. For multicore debugging, including ISP and APEX2, additional debugger and probe(S32 Debugger with S32 Debug Probe, Lauterbach, etc) will be required.
查看全文
Requirements:  SD card with installed Linux image connected to EVB (HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK ) Serial link connection between PC and EVB (HOWTO: Setup A Remote Linux Connection in S32DS for Vision ) Static IP address on PC machine Network connection between PC and EVB Use case: This settings is useful when you don't have DHCP server available or for some reason you can't connect EVB into existing network - like on this scenario:  Procedure: Setup static IP address on your PC machine - (Windows 7) click on Start -> Control Panel -> Network and Sharing center. On the left side click on "Change adapter settings" Select network interface connected to EVB ( Local area connection ) and choose "Internet protocol Version 4 (TCP/IPv4)" option and click on Properties button.   Select "Use the Following IP address" radio button and enter IP address for PC side of network connection and click on OK button.    Turn on EVB and connect to EVB via serial link using putty or any other terminal (115200 baud, 8N1). Login as the root user. Edit network interfaces configuration file by command vi /etc/network/interfaces and modify (press INS key to switch vi editor to edit mode) the file by the way as shown on next screenshot. Set IP address from range of your PC machine network settings.  Save new settings by :w command (press ESC key to switch vi editor to command mode) and exit from vi by :q command. Restart network by command /etc/init.d/networking restart  Check the IP address by command ifconfig and try ping to your PC machine.  Troubleshooting: If you can't ping to PC machine and IP address is the same as you requested - check IP address on PC side and cable connection.  If the IP address on EVB is different than you requested - check if you commented out the dhcp configuration. You may also try to reboot EVB instead of restarting network only. 
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM v2.0, Update 1             What is new? This update/service pack adds bareboard support for NXP S32K146 device into the S32 Design Studio for ARM v2.0   Installation instructions The update is available for online (Eclipse Updater) or offline (direct download link) installation.   online installation: go to menu "Help" -> "Install New Software..." dialog select predefined NXP S32 Design Studio update repository S32 Design Studio for ARM v2.0 - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2_0/com.freescale.s32arm.updatesite select all available items and click "Next" button   offline installation: go to S32 Design Studio product page -> Downloads section or use the direct download link to download the "S32 Design Studio for Power v1.2 - Update 2" file.   Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded Update 2 archive file: Select all available items and click "Next" button. This will starts the update installation.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 2          What is new? S32 SDK for Power Architecture 0.9.0 BETA for MPC574x-B-C-G and MPC574xP derivatives (see attached release notes for more details) S32 SDK  Power Architecture v0.9.0  BETA Examples - "Create S32DS Project from Example" Updated version of GNU Build tools for e200 (see the release notes attached below) Support of GHS compiler in New Project Wizard - please contact GreenHills support to obtain toolchain plugin compatible with Eclipse Neon version Updated P&E Plugin (v1.7.3.201803261737) and drivers (v12.7.0) Fixed Defects • S32DS-3506 - [e200][MPC5744P] unable to connect to secured device - addressed by adding unsecure support for MPC5744P devices • S32DS-7326 - [e200][MPC5634M] Exception occurs when accessing peripheral A registers - MMU init script error is resolved by updating the script • S32DS-7991 - [e200 2017.R1] Semihosting disabling interrupts is resolved by not disabling interrupts when stepping over specific instruction • S32DS-7177 - [MPC5634M] unable to access RAM in the debug session • S32DS-7896 - [e200] default linker sections (.got2, .jsr...) are missing in the linker script file • S32DS-3681 - [S32DS E200 B170421] Project build fail with Library support = newlib, the startup.S update to add section _fini Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
Use the New Project Wizard in S32 Design Studio to create a bare board project. The process is very straightforward, but there are some choices to be made. Which processor, toolchain, SDKs, and debugger you want supported, are the most important. However, you also have options to select on how many cores should be enabled, which C library to use,  I/O Support, FPU Support, C/C++ language. All of these are explained within the user manual, but the default settings should work for most users. In this document, we walk you through the process from start to finish.   1. Launch S32 Design Studio 2. Select File->New->S32DS Application Project or use quick button S32DS Application Project from Dashboard view 3. Enter a project name. 4. Expand the folder family and select the desired core. For example 'S32Z270 (Boot core:M33)' 5. Click Next 6. Notice there are options for I/O Support, FPU Support, Language, SDKs, and Debugger. Notice different options are supported for Debugger, depending upon the selected Processor. Also, some families have multicore projects. If you want to use single core, leave only the first Boot core checked. 7. Click Finish. The new project is generated. It contains a sample bareboard application. It is possible to build and debug this project without any changes. Add your content to this base project.  
查看全文
1. Click on the "S32 Design Studio for ARM" icon OR, from the Start menu, NXP S32 Design Studio -> S32 Design Studio for ARM -> S32 Design Studio for ARM 2. Select workspace: a. Use the default one, or b. Specify a new one Note: If you check the box "Use this as the default and do not ask again", this prompt will not appear the next time you launch S32 Design Studio for ARM. However, if later you should decide you want this to appear again, simply uncheck the box "Prompt for workspace on startup" from within the Preferences dialog window General -> Startup and Shutdown -> Workspaces. The Preferences dialog window can be opened from the Eclipse menu bar Window -> Preferences. 3. Click OK. 4. Create a new project. Go to the Eclipse menu bar and select File -> New -> New S32DS Project 5. Enter a project name. Example: FirstProject (must not contain spaces) 6. Select processor. Example: expand 'Family S32K1xx' folder, then select S32K144. 7. Click Next. 8. Select Debugger Support and Library Support. If supported, also select SDK: a. SDK for GCC b. Automotive Math and Motor Control Library Set for GCC c. FreeMASTER Serial Communication Driver 9. Click Finish 10. The new project wizard will generate the new project and then the indexer will run. It is recommended to wait until all processes complete before proceeding with any further actions.
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for S32 Platform v3.2         Austin, Texas, USA Sep 30, 2019    The Automotive Microcontrollers and Processors' Embedded Tools Team at NXP Semiconductors is pleased to announce the release of the S32 Design Studio for S32 Platform v3.2.  Here are some of its major new features: Multiple builds of the GNU tools can be installed. The SDK integration is provided with additional software packages. The SDK packages can be installed and updated with the S32DS Extensions and Updates tool. The GHS toolchain support is provided by the project wizard (available for particular devices). The CMSIS-DAP debugging is supported by particular devices. The UART communication speed of S32 Flash Tool is improved. The latest versions of P&E debugger plug-in and drivers are provided. S32 Debugger provides OS Awareness support for FreeRTOS and OSEK. S32 Debugger provides preliminary support for secure debugging with the Password and Challenge/Response authentication methods. New type of Launch Groups is defined for S32 Debugger, which allows you to create S32 Debugger specific configurations and use the new "Wait for stop on breakpoint" post launch action. The SDK migration support is provided to upgrade an SDK version attached to the project. The S32DS Extensions and Updates tool notifies about dependencies and incompatible packages. The progress bar is displayed for the S32 Debugger flash programmer. S32 Design Studio Versions   S32DS IDE for S32 Platform S32DS IDE for Arm® S32DS IDE for Power Architecture® S32DS IDE for Vision Devices Supported S32V23x S32K1xx MPC56xx S32V234 S32S247TV KEA MPC57xx   S32 Platform Devices MAC57D54H S32R2xx/S32R3xx   Integrated NXP Tools S32 Flash Tool FreeMASTER FreeMASTER DDR stress tool DDR stress tool     Integrated Configuration Tools S32 Configuration Tools Processor Expert Configuration Tool Processor Expert Configuration Tool  DDR configuration tool Pins Wizard Pins Wizard Pins Wizard Clocks configuration Peripheral/Drivers configuration   Peripheral/Drivers configuration   Peripheral/Drivers configuration   DCD/IVT configuration       DDR configuration tool       Integrated NXP Software S32 SDK S32K1 SDK S32 SDK Vision SDK FreeRTOS FreeRTOS FreeRTOS Linux BSP AMMCLib for S32V23x AMMCLib for KEA and S32K AMMCLib for MPC56xx and MPC57xx MCUs   Vision SDK KEA SDK Radar SDK Linux BSP MQX OS/MQX Drivers for MAC57D54H     Compilers: NXP GCC 6.3.1* NXP GCC 6.3.1* NXP GCC 4.9* NXP GCC 6.3.1* GreenHills GreenHills GreenHills   IAR IAR Diab     GCC 4.9*     DEBUGGERS Built-in GDB interface: S32 Debugger/S32 Debug Probe P&E Multilink/Cyclone/OpenSDA P&E Multilink/Cyclone/OpenSDA S32 Debugger/S32 Debug Probe P&E Multilink/Cyclone/OpenSDA Segger J-Link   P&E Multilink/Cyclone/OpenSDA DEBUGGERS supported: Lauterbach Lauterbach Lauterbach Lauterbach   iSystem iSystem   IAR PLS   Host Operating Systems: Microsoft Windows® 7/8/10 64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Microsoft Windows® 7/8/10 32/64-bit OS (with 32-bit binaries)  – Ubuntu 14.04, 16.04 (64 bit) – Debian 8 (64 bit) – CentOS 7 (64 bit) Vision specific tools : NXP APU Compiler     NXP APU Compiler ISP assembler     ISP assembler ISP and APEX graph tools     ISP and APEX graph tools Radar specific tools :     SPT assembler       SPT Explorer/ SPT graph tool   Complete S32 Design Studio for S32 Platform v3.2 release notes are available here.   Installation To download the installer please visit the S32 Design Studio product page download section or click the direct here.     The installer requires the Activation ID to be entered. You should receive a notification email including the Activation ID after the download of the installation package starts. The installer installs just the base tools/package. In order to start development it is necessary to install at least one Development package. Currently the only application packages available are S32S2xxTV and S32V2xx. The application packages are managed by S32DS Extensions and Updates. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space. https://community.nxp.com/community/s32/s32ds  
查看全文
CAN communication is supported in the latest version of MPC5744P Bootloader .rbf file (attached below) + Supported UART1/LINFlexD_1(OpenSDA on DevKit): PD9-PD12 pins(Speed: 115200b/s) + Supported  CAN_0 (J5 on DevKit):  PB0-PB1 pins(Speed: 500Kb/s)   Tested on the dev boards:   Development Board DEVKIT-MPC5744P MPC5744P-144DC MPC5744P-257DC Processor MPC5744P-FML09 1N15P MPC5744P-FMLQ8 0N65H PPG5744P-FMMM8 0N65H  
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 3          What is new? S32 SDK for Power Architecture 0.8.3 EAR for S32Rx7x. This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
The S32 Debugger included within the S32 Design Studio for S32 Platform IDE provides the capability to access the flash programming capabilities of the S32 Debug Probe via the S32 Debugger.   Note: currently only QSPI flashing is supported.   Preparation Install S32 Design Studio IDE  Install the Development Package for the device you are debugging. In this case, the S32R4xx development package. This package is important as the S32 Debugger support component contains the device-specific Python scripts required for initialization of the cores.   Open the application project from which the flash image will be generated. Follow the steps in HOWTO: Generate S-Record/Intel HEX/Binary file , selecting the 'Raw Binary' option. Build the project, generating the binary executable. This will be our application binary input to the IVT Tool. The IVT Tool must be used to generate the BLOB image which can be programmed to flash memory device and loaded to the RAM by the BootROM. Follow the steps in HOWTO: Use IVT Tool To Create A BLOB Image S32R45. The resulting BLOB image file is what can be flashed to the device.   Procedure Open Debug Configuration menu Select 'S32 Debugger Flash Programmer', then right-click and select New. Enter an name for the new configuration and click Add... to add the file to be flashed. Click Browse... to select the project from the workspace where the application binary is located Select the project and click OK By default, the ELF file is found. Click Search in project to select the binary file. Select the .bin file and click OK Now we must enter the base address. Typically, this could be 0, but you may have other requirements. Click OK. Now we are ready to configure the debugger connection settings. Click on the Debugger tab. Starting from the top and working our way down, click on Select device. Select the device and click OK The correct Initialization script will automatically be set. Set the Debug Probe Connection settings to match your setup. When done, click Apply To start the flashing, click Debug Flashing progress will be displayed. When complete, the Debug perspective will show at terminated thread.   Happy flashing with GDB! Note, to debug this application since it will be subsequently started by the BootROM: use 's32r45_attach.py' in the Initialization script field on the debugger tab of the Debug Configurations menu Make the following adjustments on the Startup tab within the Debug Configurations menu: Uncheck "Load image" Check “Set program counter at:” and enter the value “Reset_Handler”
查看全文
Before you can start debugging an S32DS project for S32V234 Cortex-A53 APEX2/ISP Linux target on the S32V234-EVB2, we must first setup the hardware connections and start the Linux BSP OS. 1) Connect (1) S32V234 USB Micro B port to (2) USB A port on your PC. This allow you to connect to the Linux BSP OS via a terminal program to issue commands and to obtain the IP address. 2) Insert microSDHC card (with U-boot, Linux kernel, devicetree, and root file system loaded*) into (3) the S32V234 EVB2 microSD card slot   3) Connect (1) Ethernet port on S32V234 daughter card to (2) LAN**. This will allow S32DS to communicate with the Linux BSP OS for flashing and GDB debugging.   4) Connect the power supply to (3) S234V234 EVB 5) Turn on the (4) power switch, this will start the Linux BSP OS *Instructions for preparing the SD card are provided in the VisionSDK document: ..\S32DS.x.x\S32DS\software\VSDK_S32V2_RTM_x_x_x\s32v234_sdk\docs\vsdk\S32V234-EVB_SetupGuide.pdf or refer to HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB2 Using BSP For VisionSDK  **Ensure PC is connected to LAN as well (either hardwired or wireless)
查看全文
Quick Fix is a feature of the Java editor in Eclipse which enables a user to resolve problems found in the Java code of their project. This feature is available to be used within S32 Design Studio for some problems. Such problems will be identified with the 'light bulb' icon in the description field, as shown below: For example, such problems sometimes occur when importing a project created in a previous version of S32 Design Studio, are provided from another user, or some files in a project have become corrupted. To resolve issues identified with the 'light bulb' icon, right-click on the problem and from the pop-up menu, select 'Quick Fix'.  The Quick Fix menu will appear, providing the available solutions for the problem. In most cases, there will be just one solution. Click finish to implement the fix. In some cases, more information will be required from the user to complete the fix. Complete the form to provide the additional information, then click OK. Now the problem should be resolved.
查看全文
PE Micro is not able erase unused FLASH block - typically if your application resist in Large block and Low/Mid block is used for data storage. As a workaround you can flash empty s-record into desired area.  Create new empty project for MPC5777C for flashing custom .srecord Copy empty s-record (in attachment) into project folder. If you need different address range or s-record values - feel free modify attached python script and generate your own s-record.  Open debug configuration and modify C/C++ Application to empty s-record Add custom flash algorithm nxp_mpc5777c_1x32x64k_eeprom_highspeed.pcp via Debug -> Advanced Options. Scripts are lcated in [S32DS_INSTALL_DIR]\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.3.201803261737\win32\gdi\P&E\ Start debug session. You can check if memory is rewritten properly (in this case I write zeroes to Low/Mid block): 
查看全文
The list of S32 Design Studio examples has been moved here: https://community.nxp.com/docs/DOC-341380  S32K144 EXAMPLE: S32K_printf_implementation - S32DS  EXAMPLE: S32k144 UART printf/scanf under FreeRTOS - S32DS  EXAMPLE: S32K SDK  - Function call on configurable period using LPIT timer.  EXAMPLE: FlexNVM used as code/data flash  EXAMPLE: S32K144 EEEPROM usage  EXAMPLE: S32K144 EEEPROM usage - No SDK  EXAMPLE: S32K144 .noinit section usage  For more examples and how to's: S32K1xx document & example list
查看全文
Hello,   The first official release of S32DS for Power Architecture is available in the download section of S32DS web page: http://www.nxp.com/s32ds S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB), and other open-source software. This release supports Windows 7/8/8.1 (32/64 bit), version for Linux will be released later on.   S32DS Power Architecture v1.0 main features Free of charge tool with no code size limitation (no license file required) Eclipse Luna 4.4 Framework GNU Tools for e200 processors build tools (support VLE ISA only, based on gcc 4.9.2, binutils 2.24 and gdb 7.8) Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink (with P&E GDB Server) New Project wizard to create application and library projects for supported devices Peripherals Register View   Devices supported MPC56xx MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC57xx MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5746C, MPC5745C, MPC5746D, MPC5746B, MPC5745D, MPC5745B MPC5744P, MPC5743P, MPC5742P, MPC5741P   Technical Support S32 Design Studio is supported by NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes.   Regards, Stanislav
查看全文
There are 2 errors which produce the FNP error 0 message for which we have identified solutions:   1) That activation request yields no right to a license If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution.     This issue is due to a recent event. On October 1st, 2019, Flexera made this change. Since NXP uses Flexera for product activations, we were affected.   The solution to the issue is to enable support for TLS 1.2 within your Internet Properties.   2) com.acresso.activation.handler.ServerException If you receive the following error message following an attempt to activate S32 Design Studio, this is a known issue and we have a solution. This issue is known to occur on older releases of S32 Design Studio.     The version of FlexNet Publisher (FNP) used to activate the S32 Design Studio on your PC has an issue on some users machines. While we don't fully understand what change is happening to cause this issue, we have determined that an update to the version of FNP will resolve it. We have incorporated a newer version in the 3.5 release of S32 Design Studio.   Attached is a package of files (Activation.7z) which will allow you to update the version of FNP on your machine.   Enter the following command replacing the paths as noted. It should be possible to execute from CMD window located at any path. Make sure to use the ‘/’ instead of ‘\’ and if you have any paths with spaces, then enclose the full path with “.   For 64-bit OS: C:/NXP/S32DS.3.5/jre/bin/java  -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/x64"  -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI   For 32-bit OS: C:/NXP/S32DS.3.5/jre/bin/java -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/i86" -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI   If you have no existing S32DS installation from which to use Java, then please use the attached package (CLL_FNP.11.18.0.2.zip) and follow the instructions in the included .txt file. This package only works on Windows OS 64-bit.
查看全文