Troubleshooting: S32 Design Studio exits unexpectedly or Installer rolls back immediately following activation code entry

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Troubleshooting: S32 Design Studio exits unexpectedly or Installer rolls back immediately following activation code entry

Troubleshooting: S32 Design Studio exits unexpectedly or Installer rolls back immediately following activation code entry

Problem details:

1) S32 Design Studio exits unexpectedly after workspace is selected

AND

Workspace folder .metatdata file '.log' contains Java errors.

2) Installer immediately rolls back following activation code entry

AND

Installer log contains:

==== License activation log start: ====

#

# A fatal error has been detected by the Java Runtime Environment:

#

#  EXCEPTION_ACCESS_VIOLATION (0xc0000005) at pc=0x5afc8c19, pid=10540, tid=0x000031a4

#

# JRE version: Java(TM) SE Runtime Environment (8.0_202-b08) (build 1.8.0_202-b08)

# Java VM: Java HotSpot(TM) Client VM (25.202-b08 mixed mode windows-x86 )

# Problematic frame:

# C  [cll_app.dll+0x18c19]

 

Resolution:

Trusted Storage is corrupted and needs to be re-initialized.

Windows host:

-> Delete 'C:\ProgramData\FLEXNet'

This folder may be hidden by default, so then it would be necessary to change Windows Explorer settings to show hidden items.

Linux host:

/usr/local/share/macrovision/storage

无评分
版本历史
最后更新:
‎12-12-2019 01:43 PM
更新人: