S32DS - list of Videos

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS - list of Videos

No ratings

S32DS - list of Videos

S32 Platform

Download and Install S32 Design Studio for S32 Platform v3.4 

 

S32K1

Migrating S32K1 projects from S32DS for ARM and SDK 3.0.x to S32DS 3.4 and SDK 4.0.2

A demonstration of the use of the Migration wizard in S32 Design Studio 3.4 to migrate S32K1 projects from S32 Design Studio for Arm and S32 SDK 3.0.x to S32 Design Studio 3.4 and S32 SDK 4.0.2

 

S32G2

Getting Started: Pins Tool

Getting Started: DCD Tool

Getting Started: IVT Tool

Getting Started: DDR Tool

 

S32R45

Install S32R45 Development Package

Install S32R45 Radar Extension Package

Creating And Building A Project on the S32R45 for A53, LAX and SPT Cores in S32 Design Studio

 

S32V2

Create From Example

1 | Create an ISP project from example 

A demonstration of how to load an example ISP image processing application project featuring RGB, YUV, and GS8 image formats, in the S32 Design Studio.

2 | Create an APEX2 project from example 

A demonstration of how to load an example ORB-based APEX2 image processing application project in the S32 Design Studio.

Create New Project

3 | Create a new ISP application 

A demonstration of how to create a new Debayer-based ISP image processing application project in the S32 Design Studio.

4 | Create a new APEX2 application 

A demonstration of how to create a new APEX2 image processing application project featuring upscaling and downscaling in the S32 Design Studio.

Debug

5 | ISP Debugging w/S32 Debug Probe  

A demonstration of how to setup and debug an ISP application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe.

6 | APEX2 debugging w/S32 Debug Probe 

A demonstration of how to setup and debug an APEX2 application project using S32 Design Studio, S32 Debugger, and S32 Debug Probe.

7 | APEX2 debugging with Emulator 

A demonstration of how to debug an emulated-APEX2 image processing application project in the S32 Design Studio.

8 | Debug a Linux A53 project 

A demonstration of how to debug a Linux A53 application project in the S32 Design Studio for Vision version 2.0. The example shown also includes code for APEX, but currently GDB Remote Linux only supports debug of the A53 code.

Version history
Last update:
‎01-06-2022 12:47 PM
Updated by: