S32 Design Studio for Power v1.1 - Update 1 available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for Power v1.1 - Update 1 available

S32 Design Studio for Power v1.1 - Update 1 available

Dear S32DS users,

S32 Design Studio for Power v1.1 Update 1 has been released. 

The Offline update package could be downloaded here:  

https://www.nxp.com/webapp/Download?colCode=S32DS_PA_v1.1_UP1&appType=license&location=null&Parent_n... 

 

166168_166168.pngpastedImage_9.png

For online installation please select predefined NXP repository "Help" -> "lnstall New Software..." dialog: 

${p2.metadata.repo.name} - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_1/com.freescale.s32power.updatesite

 

166166_166166.pngpastedImage_7.png

 

 

The list of changes:

  •  new compiler build 1.1.3 – see details in compiler release notes (attached)
  • MS Visual C++ 2010 Redistributable x86 included for SPT tools for Windows 10
  • Updated SPT tools:
    • ENGR00381373 - Error build after Generate SPT
    • Fixed ADD, SUB, CMP when destination register is different from src1
    • ENGR00380758 64 bits operands are not supported for spt2 on windows
  •  Updated Examples
    •  New SPT1 example for MPC5775K
    • o SingleElf_MPC5748G launch files updated with GDB command "set architecture powerpc:vle"
  • Graph Tools
    • ENGR00380255 [SPT] default graph should be created with standard includes
  • Bug fixes:
    • ENGR00375995 MPC5746C Embsys register definitons are missing SPI register set
    • ENGR00379744 SPT assembler shall have initialized 'Include paths (-I) options after MPC577xK or S32R274 project creation
    • ENGR00380796 Linker files section .spt should be corrected for SPT1/SPT2
Labels (1)
Attachments
Comments
fpn

It seems that both sites, online and offline, are down for a longer time. Any hint?

can we get SPT functionality  , in form of C code or C library files 

which will help us for analyzing ADC out with   application in IDE.

#S32DS #SPT  @iulianbulancea 

No ratings
Version history
Last update:
‎10-19-2016 07:50 AM
Updated by: