S32 Design Studio for Power Architecture v1.0 (Windows) released!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for Power Architecture v1.0 (Windows) released!

S32 Design Studio for Power Architecture v1.0 (Windows) released!

Hello,

 

The first official release of S32DS for Power Architecture is available in the download section of S32DS web page: http://www.nxp.com/s32ds

114053_114053.pngS32DS_NXP_Download.png

S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB), and other open-source software.

This release supports Windows 7/8/8.1 (32/64 bit), version for Linux will be released later on.

 

S32DS Power Architecture v1.0 main features

  • Free of charge tool with no code size limitation (no license file required)
  • Eclipse Luna 4.4 Framework
  • GNU Tools for e200 processors build tools (support VLE ISA only, based on gcc 4.9.2, binutils 2.24 and gdb 7.8)
  • Libraries included: newlib, newlib-nano and Freescale EWL2
  • P&E Multilink (with P&E GDB Server)
  • New Project wizard to create application and library projects for supported devices
  • Peripherals Register View

 

Devices supported

  • MPC56xx
    • MPC5601P, MPC5602P, MPC5603P, MPC5604P
    • MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C
    • MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B
    • MPC5606S
  • MPC57xx
    • MPC5775K, MPC5774K
    • MPC5746R, MPC5745R, MPC5743R
    • MPC5777M
    • MPC5777C
    • MPC5748G, MPC5747G, MPC5746G
    • MPC5746C, MPC5745C, MPC5746D, MPC5746B, MPC5745D, MPC5745B
    • MPC5744P, MPC5743P, MPC5742P, MPC5741P

 

Technical Support

S32 Design Studio is supported by NXP community - https://community.freescale.com/community/s32/s32ds/

For more details see the attached release notes.

 

Regards,

Stanislav

ラベル(1)
添付
コメント

Hi Stanislav,

it's great to hear the news:smileyhappy:, I have downloaded and installed the IDE with no any errors.

I created a simple project of MPC5748G with the IDE for test, all configurations are the defaults, builded to be finished with no error and warining.

but when I started to download and debug the project with Multilink-Universal FX and MPC5748G EVB(MPC574xG-256DS + X-MPC574xG-MB), I got the following errors:

Connection from "127.0.0.1" via 127.0.0.1

PE-ERROR: CAN'T READ REGISTERS. TARGET IS RUNNING

Copyright 2012 P&E Microcomputer Systems,Inc.

Command Line :C:\Freescale\S32_Power_v1.0\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.1.6.201511041643\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -interface=USBMULTILINK -speed=5000 -port=USB1 -confi

CMD>RE

Initializing.

Cannot enter background mode. Check connections. 

Error Resetting device for programming.

Reset script file not found(C:\Freescale\S32_Power_v1.0\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.1.6.201511041643\win32\gdi\P&E\).

PE-ERROR: Error downloading to the device.

PE-ERROR: CAN'T READ REGISTERS. TARGET IS RUNNING

I'm sure the driver of Multilink-Universal FX is correctly installed and the IDE automatally update its firmware when I first time plug it and launch the debug.

from the error information, it seems the reset script not found, which file is it under the path--C:\Freescale\S32_Power_v1.0\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.1.6.201511041643\win32\gdi\P&E\, should I add it manually(how to do it?).  could you help to fix the issue?

thanks~!

Enwei Hu.

Hello Enwei,

Thanks for your post!

The issue you describe is probably caused by a higher capacitance of the reset pin on certain versions of X-MPC574xG-MB EVBs.

I have figured out that boards with S/N AX15xxxxxxx may cause this issue.

Anyway there is an easy workaround: just add "Delay after Reset...." in the main core debug configuration.

I tested 250ms on multiple boards and debug works fine now.

S32DS_Power_Add_Connection_Delay.png

We are going to fix this issue by adding a default delay into MPC5748G project in the next release.

Hope it helps.

Regards,

Stanislav

Hi Stanislav,

thanks very much for your timely reply, I can debug the board now.

I find the  perpheral register value cannot be modified directly in EmbSys Registers window, can the EmbSys Registers  support the feature of online edit? if so, how can I enable it?

I think the feature of CodeWarrior 10.6 register window is very good, for it not only support online edit the register values but can display the details/functions of of peripleral and e200z core register bits.

Enwei Hu

Has access to this been pulled? I just went to the listed link. The power architecture version is not listed there.

Hi Norm,

Thanks for the heads-up!

Indeed S32 Design Studio for Power is missing on NXP web.

Currently there is Freescale->NXP migration in progress so you may observe some glitches on the web.

We apologize about inconveniences.

I'll let you know once it's available again.

Stanislav

Norm,

This issue has been fixed.

You should be able to download S32 Design Studio v1.0 for Power from NXP web again. You can use direct download link below

https://www.nxp.com/webapp/Download?colCode=S32_POWER_WIN&appType=license&location=null&fpsp=1&WT_TY...

Stan.

評価なし
バージョン履歴
最終更新日:
‎12-09-2015 06:54 AM
更新者: