S32 Design Studio for ARM v1.3 (Windows/Linux) released!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Studio for ARM v1.3 (Windows/Linux) released!

S32 Design Studio for ARM v1.3 (Windows/Linux) released!

Hello,

the new release of S32DS for ARM v1.3 is available now in the download section of S32DS web page: http://www.nxp.com/s32ds

 

170585_170585.pngpastedImage_2.png

170586_170586.pngpastedImage_3.png

The Activation code is required to install the product. The activation code is different to previous versions (v1.1/1.2).

You should get the appropriate Activation Code by a notification email which is send automatically when you proceed to the downloading:

170587_170587.pngpastedImage_4.png

What is new? 

  • New device supported: S32K144 v2.0
  • ARM64: Linaro GCC 4.9-2015.05
  • Fully integrated S32 SDK for S32K144 EAR release v0.8.2. including PinMuxing and Processor Expert configuration.
  • FreeMASTER Serial Communication driver for S32K144 family 
  • Highly Assembly Optimized version of Automotive Math and Motor Control Libraries for KEA and S32K devices v1.1.6 
  • IAR debugger support by new project wizard
  • Updated SEGGER and P&E debug plugins to the latest and greatest versions
  • Reset functionality added with P&E debugger for single core projects (KEA, S32K devices) and A5 core for MAC57D54H
  • Flash configuration supported for S32V234
  • Header files for KEA and MAC57D54H updated
  • Advanced FreeRTOS kernel aware debug support

Bug fixes

  • Project Explorer updated to correctly show active build configuration resources

 

 

Note:

The plugins to support GreenHills, IAR, iSystem, Lauterbach are not included and have to be installed from corresponding update site or installation.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎11-29-2016 09:57 AM
更新者: