S32 Design Studio 3.3 - S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0 available!

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio 3.3 - S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0 available!

S32 Design Studio 3.3 - S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0 available!

 

 

 

nxp.png

Product Release Announcement

Automotive Microcontrollers and Processors

S32 Design Studio 3.3 

S32K1xx dev package and S32 SDK for S32K1xx RTM 4.0.0

S32DS_Logo_official_2016_scaled.png  

 

 

 

What is new?

S32K1xx Development Package:

  • New Project Wizard support for S32K1xx family, including S32K14xW
  • P&E debugger support for S32K1 family
  • NXP GCC for ARM NXP GCC for Arm version 6.3 build 2017 (same as was used in S32DS for ARM 2.2)

S32 SDK for S32K1xx RTM 4.0.0:

  • S32 SDK RTM 4.0.0 package adding support for S32K1xx and S32K1xxW families, cumulative release containing also the changes present in S32 SDK for S32K1xx RTM 3.0.0, 3.0.1, 3.0.2 and 3.0.3
  • Supports S32 Design Studio for S32 Platform v3.3 with S32 Configuration tools - Pin Wizard, Clock Configuration,...
  • Supports creating project with NXP GCC for Arm Release version 6.3.1, GreenHills Multi and IAR Compiler
  • Examples for supported devices with P&E Debugger and Segger J-link support
  • Migration support for projects created in S32DS for ARM v2.2 (with Processor Expert)

For more details, please review the S32SDK_for_S32K1xx_RTM_4.0.0_ReleaseNotes.pdf attached to this notice. See below.

Installation instructions

The update is available for online (via Eclipse Updater) or offline installation 

  •  online installation: 
    • go to menu "Help" -> "S32DS Extensions and Updates" dialog 
    • select from available items and click "Install/Update" button

pastedImage_3.png

 

  • offline installation:  
    • go to S32 Design Studio v3.3 product download page: S32 Design Studio for S32 Platform -> Downloads, click 'Download' button next to S32DS for S32 Platform v3.3, then select 'S32DS.S32K1.3.3.0_D2006.zip' to download the update archive zip filepastedImage_2.png
    • Start S32 Design Studio and go to "Help" -> "S32DS Extensions and Updates"pastedImage_12.png
    • Add a new "Add.." S32DS Software Site and browse to select the downloaded update archive .zip file you downloaded in the previous steppastedImage_6.png       
      pastedImage_3.png
      pastedImage_5.png
      pastedImage_6.png
    • Select from available items and click "Install/Update" button.pastedImage_3.png

This will start the update installation process.

Labels (1)
Attachments
Comments

Hi Mike Doidge,

Customer report the 'S32DS.S32K1.3.3.0_D2006.zip' is not able to download.
I can not find this file at S32 Design Studio v3.3 product download page too.
Would you please check it?

Best Regards,
Robin

Hi Robin,

 

You can download this update package directly from the following link, no any account login required:

https://www.nxp.com/design/software/development-software/s32-design-studio-ide/s32-design-studio-for...

 

or click the link to download it: S32 Design Studio 3.1 Update 2 D2006(REV UP2_D2006)

 

Thanks~!

Best regard,

Enwei Hu.

Hi @Robin_Shen & @enwei ,

During the time since this release was published, the content of  'S32DS.S32K1.3.3.0_D2006.zip' was moved within 'S32DS3.3.0_D2008.zip'

 

image.png

Best Regards,

Mike

No ratings
Version history
Last update:
‎07-24-2020 04:44 PM
Updated by: