HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5

HOWTO: offline install S32K3 RTD 4.0.0 in S32DS v3.5

The release notes of S32K RTD usually mention which dependent software packages need to be installed. Taking SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_ReleaseNotes.pdf
as an example, we can see that the following software packages need to be installed:

SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_ReleaseNotes 1.2 Installation Design Studio.png

You must be logged into your account on NXP.com to gain access to the download link.

1. Download and install S32Design Studio 3.5: Click S32 Design Studio 3.5 – Windows/Linux -> 3.5 S32 Design Studio for S32 Platform v.3.5 -> S32DS.3.5_b220726_win32.x86_64.exe

Note: For Windows OS, the user account designated for installing S32 Design Studio for the S32 Platform must be a member of the local Administrators security group.

Download S32 Design Studio 3.5 and Update 8 step 1&2.png

 

2. Download and Install S32 Design Studio 3.5 Update 8 D2311: SW32_S32DS_3.5.8_D2311.zip (com.nxp.s32ds.update_3.5.8.20231116041033.zip)

Since the SW32K3_S32DS_3.5.8_D2311.zip downloaded in step3 already contains the files of the SW32_S32DS_3.5.8_D2311.zip in the step2, we will skip this step here.

 

3. Click S32K3 Standard Software -> Automotive SW - S32K3 - S32 Design Studio
Download and Install S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices (3.5.8_D2311): SW32K3_S32DS_3.5.8_D2311.zip  (com.nxp.s32ds.s32k3xx.update_3.5.8.20231116045533.zip)

Step3 Download SW32K3_S32DS_3.5.8_D2311.zip.jpg

Help Install New Software....png

step3 Install development package for S32K3XX SW32K3_S32DS_3.5.8_D2311.zip.jpg

Unchecking Contact all update sites during install to find required software can complete offline installation faster.

step3 Install development package for S32K3XX.jpg

 

4. Download and install S32 Design Studio 3.5.6 RTM with support for S32K39x devices(3.5.6_D2309): SW32K39x_S32DS_3.5.6_D2309.zip

Step4 Download SW32K39x_S32DS_3.5.6_D2309.zip.jpg

step4 Install development package for S32K39x.jpg

 

5. For users who need to use S32M27x(Otherwise, go to step 6), please click S32M2 Standard Software -> Automotive SW - S32M2 - S32 Design Studio
Download and Install S32 Design Studio 3.5.8 Development Package with support for S32M2xx devices(3.5.8_D2311): SW32M2_S32DS_3.5.8_D2311.zip (com.nxp.s32ds.s32m2.update_3.5.8.20231116044631.zip)

Step5 Download SW32M2_S32DS_3.5.8_D2311.zip.jpg

step5 Install development package for S32M276.jpg

 

6. Click S32K3 Standard Software -> Automotive SW - S32K3/S32M27x - Real-Time Drivers for Cortex-M
Select and install one of the updatesite for S32K3 RTD 4.0.0. 

The latest S32K3 RTD version is usually recommended. However, if you need to use Reference Software or Premium Software (such as FreeRTOS, LIN Stack, TCP/IP Stack, AWS Libraries for S32K3, S32 Safety Software Framework (SAF) for S32K3xx, Structural Core Self-Test (SCST), HSE Premium Firmware, ISELED Driver), it is recommended to install the specific version of S32K3 RTD according to their release notes.

Since there are many versions of S32K3 RTD 4.0.0, only one version of RTD will be installed here.
Download and install S32K3_S32M27x Real-Time Drivers AUTOSAR R21-11 Version 4.0.0: SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip

Step6 Download SW32K3_S32M27x_RTD_R21-11_4.0.0_D2311_DS_updatesite.zip.jpg

step6. Install S32K3 RTD 4.0.0.jpg

Then in S32DS v3.5, click File -> New -> S32DS Project from Examples and you should be able to see the example projects for S32K3 RTD 4.0.0.

S32K3XX AUTOSAR R21-11 RTD 4.0.0 D2311 Example Projects.jpg

100%が役に立ったと言っています (1/1)
バージョン履歴
最終更新日:
‎11-03-2024 10:35 PM
更新者: