HOWTO: Use RAppID BL tool with MPC5744P EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HOWTO: Use RAppID BL tool with MPC5744P EVB

HOWTO: Use RAppID BL tool with MPC5744P EVB

1. Modify your application to be compatible with RAppID BL tool. Add memory space for delay and application key in linker file (modified hello world project is in attachment):  

pastedImage_1.png

pastedImage_2.png

Add data for this sections in your app (for example in main.c file):

pastedImage_3.png

2. Flash MPC5744P.rbf file into MCU. You can create new empty project or use existing one. Start debug Configurations and Browse MPC5744P.rbf file (located in [YOUR_RAPPID_INSTALL_FOLDER]\RBF_Files. Start debug session. 

pastedImage_1.png

pastedImage_2.png

3. Modify your EVB - add jumper wire from J3-4 to J2-16  and J3-2 to J2-14. RAppID uses UART0 and to USB is connected UART1.

pastedImage_3.png 

4. Start RAppID BL tool, select COM port where EVB is connected,  choose your s-record file and Start Boot Loader:

pastedImage_4.png

附件
无评分
版本历史
最后更新:
‎12-19-2018 03:13 AM
更新人: