S32G Diagnostic Example 0.8.5 issue in S32DS 3.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G Diagnostic Example 0.8.5 issue in S32DS 3.2

1,075 Views
viktorfellinger
NXP Employee
NXP Employee

Dear community,

after importing the Diagnistic Example 0.8.5 into  S32DS 3.2 I see an error in the problem view:

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

Issue: Processor '' detected in Design Studio GCC project does not match with currently selected `S32G274A`. Target processor not supported or the computer is not on-line.
Level: Error
Type: Tool problem
Tool: McuConfiguration
Origin: DiagnosticsTest_CM7
Resource: Processor

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

Also when trying to use the ConfigTool for  clock and generate code there is an error in problem view : 

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

Issue: Clocks initialization requires the CLOCK Driver in the project.
Level: Error
Type: Validation
Tool: Toolchain/IDE project
Origin: Clocks:BOARD_BootClockRUN
Target: Toolchain/IDE project: M7_0
Resource: platform.driver.clock

>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>>

Any idea whats needs to be fixed/done to avoid this errors ? 

I'm using 

S32 Design Studio
Version: 3.2
Build id: 190924 (Update 2)

Best Regards,

Viktor

0 Replies