S32DS3.4 S32G Clocks for SERDES

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4 S32G Clocks for SERDES

1,696 Views
viktorfellinger
NXP Employee
NXP Employee

Dear support,

S32DS3.4 S32G Config Tool Clocks shows the clocks for SerDes 0 and SerDes 1 in Clock Diagram as a fixed value 100Mhz for  SerDes 0 and 125MHz for SerDes 1 - see attached snapshot ...

Hoever accoring to S32G Reference Manual the SERDES_REF_CLK is derived from PERIPH_PLL_PHI0_CLK  Clock is the same for SERDES 0 and SERDES 1.

 

Unfortunately the tool does not allow SERDES 0 clock to be set to 125MHz to be the smae as SERDE 1 which is the case for intended customer configuration.

Would it be possible to recheck the root course for this and how we could fix this ? 

 

Best Regards,

Viktor

 

 

0 Kudos
0 Replies