S32DS3.4 Pins configuration tool bugs for MAXQFP100/172 S32K314

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4 Pins configuration tool bugs for MAXQFP100/172 S32K314

1,142 Views
guenter_loettrich
NXP Employee
NXP Employee

Hi all,

there is an issue with the pin muxing configuration tool in S32DS3.2 when selecting S32K314 and with MAXQFp100 package. Using RTD 0.8.1

If you chose MAXQFP100 then still the MAXQFP172 is displayed and the pinmuxing settings do not reflect the 100pin version. Also the picture of MAXQFP172 is not shown correctly.

Thanks for checking and correction.

MAXQFP172:

guenter_loettrich_0-1614774220911.png

MAXQFP100:

guenter_loettrich_1-1614774290240.png

 

br

Guenter

0 Kudos
0 Replies