what is the process geometry (nano meter specs) for MC9S12 CPUs?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

what is the process geometry (nano meter specs) for MC9S12 CPUs?

1,159件の閲覧回数
tommctaggart
Contributor I

What is the process geometry size for the MC9S12 CPU, please?

ラベル(1)
0 件の賞賛
返信
1 返信

1,045件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi Tom,

The most of the MC9S12 device families which are active and in production are based on 180nm process technology such as S12XE, S12G and MagniV devices based on S12Z core such as S12ZVM, S12ZVL, S12ZVC etc.

Some other families are based on 250nm process technology such as S12A/B/C/D/E, S12P, S12XD and few more.

Have a great day,
iggi

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信