what is the procedure to handle unused port pins of part MC9S12XET256MAG ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

what is the procedure to handle unused port pins of part MC9S12XET256MAG ?

1,076 次查看
kumara
Contributor I
0 项奖励
回复
2 回复数

915 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

The http://www.nxp.com/docs/en/application-note/AN3262.pdf written for S12XD family devices can be used to better understand design. Of course, there are some differences between devices but the HW design is almost the same and technical approach is common.

The Chapter 14 describes Managing Unused Pins.

Best regards,

Ladislav

0 项奖励
回复

915 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Unused pins can be configured as inputs or outputs. But because internal pull resistors are active only in the input mode, it is better to set them as inputs and enable pullups. Many pins have pullups enabled by default, out of reset.

 

Regards,

Daniel

0 项奖励
回复