what is the procedure to handle unused port pins of part MC9S12XET256MAG ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

what is the procedure to handle unused port pins of part MC9S12XET256MAG ?

1,083 Views
kumara
Contributor I
0 Kudos
Reply
2 Replies

922 Views
lama
NXP TechSupport
NXP TechSupport

Hi,

The http://www.nxp.com/docs/en/application-note/AN3262.pdf written for S12XD family devices can be used to better understand design. Of course, there are some differences between devices but the HW design is almost the same and technical approach is common.

The Chapter 14 describes Managing Unused Pins.

Best regards,

Ladislav

0 Kudos
Reply

922 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

Unused pins can be configured as inputs or outputs. But because internal pull resistors are active only in the input mode, it is better to set them as inputs and enable pullups. Many pins have pullups enabled by default, out of reset.

 

Regards,

Daniel

0 Kudos
Reply