When we put a cellphone close to our board ,it is likely that the mcu will reset, but not all the phone can cause this problem, and only when the phone is in calling someone and his phone doesn't have alarm;
our board using mc9s12hy64 mcu, using outside 8m frequency crystal oscillator, an the software config the mcu using a frequency of 64M ,so the bus clock is 32M , the software config init code as below:
{
unsigned char i = 255;
CPMUPROT = 0x26;
CPMUCLKS_PLLSEL = 1;
CPMUREFDIV = 0x80; /* Config fREF 4M */
CPMUSYNR = 0x43; /* Config fVCO 64M */
CPMUPOSTDIV = 0x00; /* Config fPLL 64M fBus 32M */
CPMUOSC_OSCE = 1; /* enable ext OSC */
do{
i--;
}while((!CPMUFLG_UPOSC || !CPMUFLG_LOCK) && (i));
/* wait for ext osc to stabilize and pll to lock */
CPMUFLG = 0xFF;
CPMUCLKS = 0x81; /* RTI COP clock source is oscclk */
CPMUCOP = 0x46;
/* watchdog reset time 1.04S */
CPMURTI = 0xF9; /* RTI Time 0.25s */
CPMUINT_RTIE = 0; /* enable RTI interrupt */
while( CPMUCLKS != 0x81 )
{
CPMUCLKS = 0x81;
}
CPMUPROT = 0x01; /* Protect pll clock */
}
Can anyone give an advise or give me some direction?