Hello.all
I am working with MM9Z1_638D1 .freshman. So far I was even unable to download the procedure.When i downloaded the procedure with CW10.6,meeted
Then i click “yes”,and meet
and then i follow the prompts,
but meet that"device is secure,erase to unsecure"again,i click yes again and meet
and i click retry ,but it dosent work
If you are using the KIT9Z1J636EVM and the OSBDM that is on the EVM, switch S1 must be set as follows:
If an External BDM tool is being used (i.e. USB Multilink), S1 must be configured as follows:
Hope this helps.