some example about the FOC dead-time compensation?my mcu is s12ZVML128,andI setPMFCCTL_ISENS = 0x10;

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

some example about the FOC dead-time compensation?my mcu is s12ZVML128,andI setPMFCCTL_ISENS = 0x10;

3,480 Views
Clarkhe
Contributor I

hi。

i have some questions about the dead-time compensation?my mcu is s12ZVML128,

I tried the current zero crossing detection compensation and register detection compensation method, the effect is not good, request help, thank you

 

Thanks!

 

void pmf_init(void)
{
PMFCFG2_REV0 = 1; // 01 PWM generator A generates reload event.
PMFCFG2_REV1 = 0;

PMFMODA = 2500; // pwm frequency to be 20 kHz
PMFDTMA = MOS_DEAD_TIME; // dead time of pmf to be 0.75 us

PMFCCTL_ISENS = 0x10; // 死区补偿方法

PMFVAL0 = PMFMODA >> 1; // set the output duty to be 50%
PMFVAL2 = PMFMODA >> 1;
PMFVAL4 = PMFMODA >> 1;

PMFENCA_LDOKA = 1; // apply PMF Modulo value

PMFICCTL_PECx = 0x7; // Enable Double Switching
PMFCINV = 0x15;

PMFCFG2_MSK = 0x3F; // Disable PWM at the output

PMFENCA_PWMENA = 1; // Enable PWM

PMFENCA_PWMRIEA = 1; // Reload Interrupt - Used for sampling period generation

PMFENCA_GLDOKA = 1; // 0 = Local LDOKA controls buffered registers / 1 = external Load OK controls buffered registers
PMFFQCA_LDFQA = 1; // Reload every TWO PWM, 10KHZ,page588
}

0 Kudos
Reply
6 Replies

3,396 Views
pachamatej
NXP Employee
NXP Employee

Hello,

I believe there is a mistake in the assignment:


PMFCCTL_ISENS = 0x10; // assigning hex number of 0x10, leading to 0b000010000 being assigned to two-bit fieldIf you

If your intention is to use mode 10 (Current status sample correction on inputs IS0, IS1, and IS2 during deadtime), please use


PMFCCTL_ISENS = 0b10;

or


PMFCCTL_ISENS = 0x02;

or


PMFCCTL = 0x20;

instead.

Let me know if it works for you.

 

Best regards,

Matej

0 Kudos
Reply

3,450 Views
Clarkhe
Contributor I

/* 死区补偿 -寄存器换向标志位检测换向 */
if(PMFDTMS_DT0 == 0)//正电流
{
f16pwm->f16Arg1 = MLIB_AddSat_F16(f16pwm->f16Arg1, DeadTime_H);
}
if(PMFDTMS_DT1 == 1)//负电流
{
f16pwm->f16Arg1 = MLIB_SubSat_F16(f16pwm->f16Arg1, DeadTime_L);
}
if(PMFDTMS_DT2 == 0)//正电流
{
f16pwm->f16Arg2 = MLIB_AddSat_F16(f16pwm->f16Arg2, DeadTime_H);
}
if(PMFDTMS_DT3 == 1)//负电流
{
f16pwm->f16Arg2 = MLIB_SubSat_F16(f16pwm->f16Arg2, DeadTime_L);
}
if(PMFDTMS_DT4 == 0)//正电流
{
f16pwm->f16Arg3 = MLIB_AddSat_F16(f16pwm->f16Arg3, DeadTime_H);
}
if(PMFDTMS_DT5 == 1)//负电流
{
f16pwm->f16Arg3 = MLIB_SubSat_F16(f16pwm->f16Arg3, DeadTime_L);
}

0 Kudos
Reply

3,449 Views
Clarkhe
Contributor I

QQ图片20201225082305.jpg

0 Kudos
Reply

3,449 Views
Clarkhe
Contributor I

Current waveform after dead time compensation

0 Kudos
Reply

3,479 Views
Clarkhe
Contributor I

IMG_2109.JPG

0 Kudos
Reply

3,448 Views
Clarkhe
Contributor I

Current waveform before dead time compensation

0 Kudos
Reply