s12g: SWI command resets to 0x0 rather than address at reset vector

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

s12g: SWI command resets to 0x0 rather than address at reset vector

跳至解决方案
1,794 次查看
ilya_r
Contributor III

working with the s12g128 processor:

 

the SWI reset command sends mirco to address 0x0 rather than the address programmed in the reset vectors @ 0xFFFA, 0xFFFC or 0xFFFE

标签 (1)
0 项奖励
回复
1 解答
1,480 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

I am not sure I understand the behavior you described.

The SWI is not reset oriented.

(Vector base + 0x00F8) Unimplemented opcode trap

(Vector base + 0x00F6) Software interrupt instruction (SWI) or BDM vector request

The software interrupt (SWI) instruction initiates synchronous exception processing. First, the return PC value is stacked. After CPU context is stacked, execution continues at the address pointed to by the SWI vector.

I have attached an example I have tested the functionality. It worked without any problems. G128-CPU-SWItest-CW51.zip

Best Regards,

Ladislav

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,481 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

I am not sure I understand the behavior you described.

The SWI is not reset oriented.

(Vector base + 0x00F8) Unimplemented opcode trap

(Vector base + 0x00F6) Software interrupt instruction (SWI) or BDM vector request

The software interrupt (SWI) instruction initiates synchronous exception processing. First, the return PC value is stacked. After CPU context is stacked, execution continues at the address pointed to by the SWI vector.

I have attached an example I have tested the functionality. It worked without any problems. G128-CPU-SWItest-CW51.zip

Best Regards,

Ladislav

0 项奖励
回复
1,480 次查看
ilya_r
Contributor III

Thanks.

Based on the some of the AN's and TP's I read I got the wrong impression that SWI was a software reset request.

0 项奖励
回复