seen as below
i call for an interrupt function of timer , but the interrupt was recognized as normal code rather than a keyword(like void, while).
in consequence, the build result failed with "function has no prototype "
can anyone help , thx in advance
Hello,
This is caused by the compiler option - require prototype. I'd recommend you to declare ISR routine prototype:
void interrupt Timer();
Hope it helps.
Stan