mm9z1-638: PCR_SR register question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mm9z1-638: PCR_SR register question

987件の閲覧回数
gumu
Contributor V

Dear Sir:

We have a question about the booting reason after coming up from the stop mode. The value of the reset reason register is 0x0908, according to the PCR_SR register description, showing the HVRF and WLPMF waking up. While we can understand the WLPMF wake-up reason, why is the HVRF wake-up reason set? Is this normal?

0 件の賞賛
返信
2 返答(返信)

947件の閲覧回数
gumu
Contributor V

Hi @Q_man ,

Sometimes, we receive a reset reason of 0x100. Please refer to my other post for the description.

MM9z1-638:no wakeup reason - NXP Community

 

0 件の賞賛
返信

955件の閲覧回数
Q_man
NXP Employee
NXP Employee

Hi Gumu,

The 0x0908 makes sense and is expected!
The PCR register latches all conditions since last clearing of bits:

- device did wakeup based on PTB4 (WLPMF and WUPTB4F)

- device saw low voltage condition on VDDH (voltage of D2D Interface). VDDH is turned off during STOP mode.

W.

0 件の賞賛
返信