mc9s12hy64 crystal gain control, Where is the register, I can't find and use it

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mc9s12hy64 crystal gain control, Where is the register, I can't find and use it

1,134 次查看
hongjianzhang
Contributor III

We now have problems in using this mcu, that is the EMI ablity is weak,and an engineer tell us this mcu have oscillator gain control function, but in the datasheet we didn't find it;  

 

Can anyone tell us?

标签 (1)
2 回复数

953 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

our older MCUs contains selection option of two different Pierce oscillator circuitries. They are "loop controled" and "full swing". This MCU, however, contains only loop controlled option and internal RC oscillator. If you do not need absolute exact timing, as necessary for example for CAN, you can use internal RC oscillator as a clock source for your application.

There is no gain control feature implemented.

Following also relates to my previous response. Do you have TEST pin grounded. I hope you have all unused pins correctly connected as well as all unused interrupt solved with some interrupt catcher to be able to catch all unexpected event (especially during debugging).

Interrupt catcher = all interrupts have own service routine which calls common function with identification number as a parameter. Then it is enough to have breakpoint set within the common function to catch all unexpected event.

Best regards,

Ladislav.

953 次查看
hongjianzhang
Contributor III

Thank you for your answer, we will try another way

0 项奖励
回复