masserase memory map

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

masserase memory map

970 次查看
Neo_zhang
Contributor II

CW execute masserase, which part the memory has been erased?  both EEPROM and flash or just the flash ?

0 项奖励
回复
2 回复数

953 次查看
stanish
NXP Employee
NXP Employee

Hi,

Could you please specify the target MCU you are using?

In case it is S12(x) family there is an option to enable/disable erasing of EEPROM (go to File -> Configuration dialog - where you can specify which flash memory blocks should be erased:

stanish_0-1709902761322.png

If you use S12z the debug will erase just Program FLASH. in order to program EEPROM you should use Flash Programmer component (Target Task): 

stanish_1-1709903067485.png

 

Hope it helps.

Stan

 

0 项奖励
回复

950 次查看
Neo_zhang
Contributor II

My target MCU  is MC9S12DT256, can I edit 0x000 - 0x3FF registers region and 0x1000 - 0x3FFF RAM and how to do it?

0 项奖励
回复