low vls error in magniv

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

low vls error in magniv

2,003件の閲覧回数
steven_zhang
Contributor V

my customer test the Stall  status for his DC motor board, gotting the low VLS error .

we checked the voltage of VLS_out =11V ,the setting of GVLSLVL=0,  

is there  any other reason for the error?

 

0 件の賞賛
返信
1 返信

1,992件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

It is necessary the error flag clear when the MCU is started/powered up. It is possible that in this case the voltage is evaluated sooner than it is in correct range.

However, if the error appears during running mode then it is necessary to measure conditions by setting voltage trigger at the oscilloscope to be able investigate the reason of the voltage drop.

Moreover, this drop, if during run, should probably also be visible at overcurrent protection.

TO measure VLS_OUT is not enough there must be deeper investigation and measurements.

Best regards,

Ladislav

0 件の賞賛
返信