how to set the runtime in setting of PPAGE register is used for paging

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to set the runtime in setting of PPAGE register is used for paging

807件の閲覧回数
mengzhang
Contributor II

We have a project which need to use expended page. we have set the file of project.prm ,for example internal ram or rom,and external ram. so i need to set the option of compiler for hc12. Some freescale FAE tell us that the option "PPAGE Register is used for paging" should be set first. but the envirement shows that PPAGE Register is used for paging(enter [0xaddr|RUNTIME]) the question is that how to set this option?how to set this RUNTIME? We are directly  writing "RUNTIME" into the blank.but It is failed to visit the right page which need to be visited.

41654_41654.JPGruntime.JPG

ラベル(1)
0 件の賞賛
返信
1 返信

723件の閲覧回数
iggi
NXP Employee
NXP Employee

The same topic you've opened in CodeWarrior space, so we can continue the discussion there:

how to set runtime in setting of PPAGE register is used for paging in code generation

0 件の賞賛
返信