how to reduce the current of High side gate driving on S12ZVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how to reduce the current of High side gate driving on S12ZVM

ソリューションへジャンプ
1,151件の閲覧回数
ikkishingu
Contributor II

Hello,

 

S12ZVM has the function the slew rate control of high side gate driving, GSRCHS,

 

and the range is as below,

 

Iref(min)=10uA -> Iout = 10u * 36 * 450 = 162mA

Iref(max)=80uA -> Iout = 80u * 36 * 450 = 1.29A

 

If we would like to reduce the current further than 162mA, is there any good idea?

 

Best Regards,

Ikki

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,002件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

Looking at the concept of the FET Pre-Driver in the S12ZVM ref. manual, a way to decrease Iref and Iout is to decrease voltage on VBS. But, this can lead to some other consequences.

Another way is to put a resistor on HG pin (and power FET's gate). With this approach the max Iout current will be decreased as well.

FET pre-driver concept.PNG.png

Regards,

iggi

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,003件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

Looking at the concept of the FET Pre-Driver in the S12ZVM ref. manual, a way to decrease Iref and Iout is to decrease voltage on VBS. But, this can lead to some other consequences.

Another way is to put a resistor on HG pin (and power FET's gate). With this approach the max Iout current will be decreased as well.

FET pre-driver concept.PNG.png

Regards,

iggi

0 件の賞賛
返信
1,002件の閲覧回数
ikkishingu
Contributor II

iggi-san,

Thank you for your response.

To decrease voltage on VBS would not be good for the BLDC stable rotation,

so I understand that the only way is to put a resistor on HG pin and there is no way to reduce the gate drive current by itself.

Ikki

0 件の賞賛
返信