hello, I hope that someone can help me on this issue: i w...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

hello, I hope that someone can help me on this issue: i w...

1,872 次查看
masxx
Contributor I
hello,
I hope that someone can help me on this issue:
i want to connect my 68hc12 microcontroller to a gsm modem through serial rs232. My current status is as follows:
I can transmit data from microcontroller to hyperterm on PC
I can talk to my gsm modem through the hyperterminal
However, the gsm does not respond at all when i try to transmitt data to it through microctroller

I have a dragon 12 board that cointains MC9S12DP256. My gsm modem is westermo GD-01

Thank you
标签 (1)
0 项奖励
回复
2 回复数

1,066 次查看
masxx
Contributor I
thank you ... the system is working now
0 项奖励
回复

1,066 次查看
JimDon
Senior Contributor III
You probably need a 'null' modem cable when connecting the Dragon to the modem.
Since dragon and the modem both have the same pin out based on what you stated, pins 2 & 3 need to be cross connected.

Note that a "lap link" cable will work as well.

0 项奖励
回复