external EEPROM with a MC9S12P64VLH?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

external EEPROM with a MC9S12P64VLH?

808 Views
marchandthomas
Contributor I

Hello ,

 

do you know if there is an existing schematic for connect an external EEPROM with a MC9S12P64VLH?

I think we can use a ATMEL25640 on the Pin 58 ,57,56,55 (MISO0,/SSO,MOSI0,/SCK0). Do you know the best circuit?

Thanks you.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

741 Views
iggi
NXP Employee
NXP Employee

Hi,

The S12P features SPI module (MISO0,/SSO,MOSI0,/SCK0) as well, so you can use this serial interface for external EEPROM.

Below post can be of help as an alternative:

External Serial EEPROM | Freescale Community

Moreover, there is an appnote for S12P devices about EEPROM emulation (it comes with the SW driver), so you might not need to use external EEPROM:

AN4483, Emulated EEPROM Routines for the S12P Family - Application Notes

AN4483SW

Regards,

iggi

0 Kudos
Reply