dsp  and the microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

dsp  and the microcontroller

2,916 次查看
cpo
Contributor I
Some years back (1990s?), Motorola, as it then was, produced a fine manual that they distributed with the MC68HC16 development kit. It was called 'Digital Signal Processing and The Microcontroller'. Does anyone have a copy that they no longer need, or can point me to where I might obtain one.  The authors were Mark McQuilken and James P. LeBlanc.    Many thanks
标签 (1)
0 项奖励
回复
5 回复数

1,386 次查看
JimDon
Senior Contributor III
Did you try google? I get lots of hits.
Looks like it will cost you about 100.00 from amazon used...


Message Edited by JimDon on 2008-01-17 03:31 PM
0 项奖励
回复

1,386 次查看
JimDon
Senior Contributor III
Well this one was published by Motorola University, so maybe you (or your source) got the authors name wrong.
Pretty unlikely (though possible, I suppose) Motorola would publish two books with the exact same title.
Perhaps this book is based on a papaer they wrote, but you would think they would get autohor credit.
Further, there is no reference to ANY books by Mark McQuilken and James P. LeBlanc, except on a very old new group from 1995. I am will to bet he got it wrong, and this is the book that was in the kit.

Also, this book got excellent reviews, now I want a copy.



Message Edited by JimDon on 2008-01-17 04:24 PM
0 项奖励
回复

1,386 次查看
allawtterb
Contributor IV
If you are sure that those are the authors you could always contact one of them.  I believe this is the James P. LeBlanc that you are referring to:
http://www.ltu.se/csee/research/signalbehandling
 
0 项奖励
回复

1,386 次查看
cpo
Contributor I
Thanks for that link. He is definitely one of the Authors, as is the other person I sited.... I have a copy of the book in front of me, but require a second copy. I will sent out a quiet enquiry to him.
0 项奖励
回复

1,386 次查看
cpo
Contributor I
Thanks for your response... Amazon search shows the right title, but a different author. This book has no ISBN number. As far as I'm aware it was never for sale but put out by Motorola as a primer for would-be DSP engineers.
0 项奖励
回复