co-relation between instruction and clock/bus cycle

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

co-relation between instruction and clock/bus cycle

1,977 次查看
applejuice5
Contributor I

for S12 family there is mentioned core clock and bus clock, which is half the core clock.

now each instruction cycle is one bus clock or core clock ?

标签 (1)
0 项奖励
回复
3 回复数

1,344 次查看
jsmcortina
Contributor III

If you haven't already seen it, then take a look at the S12XCPU datasheet. That lists each instruction and its cycle count.

 

Looks like S12XCPUV1.pdf is still the current version.

 

James

0 项奖励
回复

1,344 次查看
MJW
NXP Employee
NXP Employee

Hello,

 

the correct version of the CPU reference manual depends on the actual MCU family used:

 

* most S12 devices generally refer to the S12CPUV2 Reference Manual (S12CPUV2.pdf, latest Rev as of today: 4.0)

 

* some S12X (e.g. S12XD) refer to the S12XCPUV1 Reference Manual (S12XCPUV1.pdf, latest Rev as of today: 1.01)

 

* most S12X (e.g. S12XS, S12XF, S12XE) and recent S12 devices (e.g. S12P) refer to the CPU12/CPU12X Reference Manual (S12XCPUV2.pdf, latest Rev as of today:1.03)

 

This last document mentioned above actually describes the all existing ISA versions for CPU12 and CPU12X.

 

HTH,

MJW

 

0 项奖励
回复

1,344 次查看
kef
Specialist I

Shortest instruction (like NOP) take one bus cycle.

0 项奖励
回复