cannot understand SYS instruction for S12XE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

cannot understand SYS instruction for S12XE

1,584件の閲覧回数
Xbot
Contributor II
hi,
 
i'm having a hard time understanding the purpose of the SYS instruction. this is supposed to an MPU call. is this an interrupt call where you can enter supervisor state? how about when i want to set the descriptors for XGATE code execution, how do do it?
 
there is also interrupt vectors for access errors ?
ラベル(1)
0 件の賞賛
返信
1 返信

803件の閲覧回数
Steve
NXP Employee
NXP Employee
SYS is an additional "software interrupt" that does the same kind of thing as SWI. It was added because SWI is already heavily used in debugging environments. The intent of SYS is to provide a separate software interrupt for use by the system that will not cause confusion and difficulties for development tools.
All interrupts including SYS return you to supervisor state.
Read AN3242 for more information about the MPU and SYS and Supervisor and User State.
0 件の賞賛
返信