can anybody provide the example project for s12g to wake up from the sci?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

can anybody provide the example project for s12g to wake up from the sci?

802件の閲覧回数
steven_zhang
Contributor V

can anybody provide the example project for s12g to wake up from the sci?

ラベル(1)
0 件の賞賛
返信
1 返信

663件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Steven,

Please look at my example code GN32-SCI_wake_up_from_stop-CW51 here:

https://community.freescale.com/docs/DOC-93792

SCI edge is here used for wake-up from stop mode.


I hope it helps you.

Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信