ad convertion - MC9S12XDT512MAA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ad convertion - MC9S12XDT512MAA

2,677 Views
Gerald1
Contributor I
hi,

i have one question to the ad convertion:
if i set:
AD_CTRL_REG1 = 0x01;
AD_CTRL_REG4 = 0x68;
AD_CTRL_REG5 = 0xb0;

it will start the convertion if the signal on AN00 changes? is there a possibility to manually start the convertion by setting a ad_start flag?
 
 
 
 
 
 
Added p/n to subject.


Message Edited by NLFSJ on 2008-02-11 01:59 PM
Labels (1)
0 Kudos
Reply
2 Replies

875 Views
DPB
NXP Employee
NXP Employee
Hello

If ETRIGE (ATDCTL2[2]) is clear then a conversion sequence is started simply by writing to ATDCTL5.

Only when ETRIGE is set, does the ATD use external triggers as defined by ATDCTL1.

DPB
0 Kudos
Reply

875 Views
Gerald1
Contributor I
oh, your post got deleted?! hmmm
0 Kudos
Reply