Why the port pins PS0 and PJ0 are not getting driven High on S12ZVCA Evaluation board?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why the port pins PS0 and PJ0 are not getting driven High on S12ZVCA Evaluation board?

1,600件の閲覧回数
bhushanpatil
Contributor I


Hi,

I am using S12ZVC Evaluation Board.(S912ZVCA19F0WKH [magni v 192kB])

It has been observed that the port pins PS0 and PJ0 when configured as GPIO(Outputs) and forced to logic level HIGH

by writing to the respective Data Direction Register(DDRx) and Port Data Register(PTx) does not reflect into HIGH level on board.

Instead of both the pins (PS0 and PJ0) driven to 5 Volts the behavior observed was as mentioned below:

Physical Voltage on PS0 Pin -  3 Volts

Physical Voltage on PJ0 Pin - 0.1 Volts(Approx)

 

 

Guidance on the deviation of the results will be helpful !

 

Thanks & Regards,

Bhushan Patil

ラベル(1)
0 件の賞賛
返信
1 返信

1,451件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Bhushan,

It seems that you asked twice on the same, please look at my answer in you second thread:

https://community.nxp.com/message/820534#comment-820534

Best regards

Radek

0 件の賞賛
返信