Whether the ADC sampling voltage is too high will breakdown the chip

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Whether the ADC sampling voltage is too high will breakdown the chip

跳至解决方案
1,163 次查看
AsaZJP
Contributor III

Hi 

         The chip we use is MC912ZVL128 of s12z,If the sampling voltage of the ADC pin reaches 11v instantaneously (the duration is about 50us), will it affect the 5v output of the chip,Short-circuiting the 5v output circuit inside the chip.

best wishes.

Asa.Zhai

0 项奖励
回复
1 解答
1,150 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

you must use the MCU within specifications. Such usage has cumulative effect. The solution is correctly designed filter at the ATD input.
https://www.nxp.com/docs/en/application-note/AN2429.pdf

Best regards,
Ladislav

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,151 次查看
lama
NXP TechSupport
NXP TechSupport

Hi,

you must use the MCU within specifications. Such usage has cumulative effect. The solution is correctly designed filter at the ATD input.
https://www.nxp.com/docs/en/application-note/AN2429.pdf

Best regards,
Ladislav

0 项奖励
回复