What is the difference between MFR4310 and SFR4310?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between MFR4310 and SFR4310?

2,189件の閲覧回数
stephenchen
Contributor II

What is the difference between MFR4310 and SFR4310? What should I consider when I use the different "4310"?

ラベル(1)
タグ(2)
0 件の賞賛
返信
4 返答(返信)

1,936件の閲覧回数
iggi
NXP Employee
NXP Employee

Hi,

the only difference is that SFR4310 is Automotive graded part, while the MFR4310 is general market part.

The form, fit and functionality is the same.

So, the selection between these two depends on end application.

Regards,

iggi

1,936件の閲覧回数
stephenchen
Contributor II

Hi,

The operating temperature is the same too?

I think that "SFR4310" is more reliable,is that right?

thanks.

0 件の賞賛
返信

1,936件の閲覧回数
iggi
NXP Employee
NXP Employee

Well, the part number specifies ambient temperature which is the same for both: -45°C to +125°C.

Both parts are reliable. As i said previously, if the end application will be Automotive (used in cars, tracks etc), then you should use SFR4310 part.

1,936件の閲覧回数
stephenchen
Contributor II

thank you

0 件の賞賛
返信