What is the difference between MFR4310 and SFR4310?

cancel
Showing results for 
Search instead for 
Did you mean: 

What is the difference between MFR4310 and SFR4310?

326 Views
stephenchen
Contributor II

What is the difference between MFR4310 and SFR4310? What should I consider when I use the different "4310"?

Labels (1)
Tags (2)
0 Kudos
4 Replies

73 Views
iggi
NXP Employee
NXP Employee

Hi,

the only difference is that SFR4310 is Automotive graded part, while the MFR4310 is general market part.

The form, fit and functionality is the same.

So, the selection between these two depends on end application.

Regards,

iggi

73 Views
stephenchen
Contributor II

Hi,

The operating temperature is the same too?

I think that "SFR4310" is more reliable,is that right?

thanks.

0 Kudos

73 Views
iggi
NXP Employee
NXP Employee

Well, the part number specifies ambient temperature which is the same for both: -45°C to +125°C.

Both parts are reliable. As i said previously, if the end application will be Automotive (used in cars, tracks etc), then you should use SFR4310 part.

73 Views
stephenchen
Contributor II

thank you

0 Kudos