Hi,
Sorry, one more question. I read the chapter on the Pierce oscillator and it looks like the hardware engineer designed the board according to Figure 6-4 on page 277 External Clock Connections. The XTAL pin is not connected in our design and the EXTAL pin is connected to an ECS brand oscillator.
Is this a problem? Also, it appears that the VDDPLL and XFC pins are connected according to Figure 1.7 - PLL Loop Filter Connections. Does this need to be changed if following Figure 6-4?
Thanks in advance for the answer.