Using EEPROM at 0xC00 in the S12XEP MPU for storage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using EEPROM at 0xC00 in the S12XEP MPU for storage

ソリューションへジャンプ
1,320件の閲覧回数
wb9ypa
Contributor II

I tried to use the EEPROM space between 0xC00 and 0XFFF, but, when power is removed and re-applied the memory loses what was previously stored.  The datasheet states that writing to EEPROM is automatic so I must be missing something here.  I have tried finding assembly language examples using the XEP's internal D-FLASH memory and the explanation given in the data sheet in that section appear to be cryptic so it's difficult to put all of the pieces together. I started coding based on the simple flow chart on page 1173 of the S12XFTM1024K5V2 module documentation, but understanding how to use the FCCOB register or setting a "Field Margin Level" is beyond my comprehension without further explanation.  If there are any reasonable examples of how to read and write to the EEPROM at the address starting at 0xC00 then I would be very happy.  I have no one else to turn to for help with this. I hope I am not too hopeless for anyone to help me with this.

ラベル(1)
1 解決策
1,043件の閲覧回数
wb9ypa
Contributor II

Thank you Ladislav,

This was a great help to me and I appreciate your help with all of this!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,043件の閲覧回数
lama
NXP TechSupport
NXP TechSupport

Hi,

I can recommend the application notes:

 

cache.nxp.com/assets/documents/data/en/application-notes/AN3490.pdf

cache.nxp.com/assets/documents/data/en/application-notes/AN3743.pdf

 

There are two examples for EEEPROM in the packages at https://community.nxp.com/docs/DOC-329209    (search for EEE in the name of examples)

 

BTW, C00~FFF is only a Ram which can be used as a memory space (interface) for EEPROM. You can find also the example how it is used as a RAM only.

 

I believe these examples will help you to understand.

 

Best regards,

Ladislav

1,044件の閲覧回数
wb9ypa
Contributor II

Thank you Ladislav,

This was a great help to me and I appreciate your help with all of this!

0 件の賞賛
返信