Use the S12ZVML-MINIBRD Board to change the motor speed

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Use the S12ZVML-MINIBRD Board to change the motor speed

跳至解决方案
1,201 次查看
519315342
Contributor I

Can I modify the code to change the motor speed?

what is the code to control the speed of the motor ? And how to modify the code can control the motor speed?

标签 (1)
0 项奖励
回复
1 解答
868 次查看
stanish
NXP Employee
NXP Employee

Hi,

as far as I know this motor control application can be controled from FreeMASTER visualization tool via OSBDM serial COM. (see the screenshot below)

S12ZVM_FreeMASTER_control.png

FreeMASTER .pmp file should be part of the demo application.

Hope it helps.

Stan

在原帖中查看解决方案

0 项奖励
回复
1 回复
869 次查看
stanish
NXP Employee
NXP Employee

Hi,

as far as I know this motor control application can be controled from FreeMASTER visualization tool via OSBDM serial COM. (see the screenshot below)

S12ZVM_FreeMASTER_control.png

FreeMASTER .pmp file should be part of the demo application.

Hope it helps.

Stan

0 项奖励
回复