Tool qualification of Codewarrior V11.1 and FreeMaster 3.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Tool qualification of Codewarrior V11.1 and FreeMaster 3.1

Jump to solution
1,614 Views
magniv-co
Contributor I

We are developing a MCU( S12ZVML) and need to prove tool qualification of Codewarrior v11.1& FreeMASTER3.1.  As I know, there is no certification but I heard that NXP provide customers proven in use documents instead so we try to explain "Increased confidence from use" for qualification. Can I receive the customers proven in use documents?

0 Kudos
Reply
1 Solution
1,572 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I sent you CW11.1 Proven In Use document via email.

There is no such document for FreeMaster as this is just a monitoring or debugging tool.

Proven In Use is only required for tools that affect and can change the embedded code or processor.

 

Best regards,

Daniel

View solution in original post

2 Replies
1,554 Views
magniv-co
Contributor I

I really appreciate your reply. It was very helpful to me

In case of FreeMASTER, I have to find another method to prove qualification. but it's ok

thank you~ So! much!

0 Kudos
Reply
1,573 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello,

I sent you CW11.1 Proven In Use document via email.

There is no such document for FreeMaster as this is just a monitoring or debugging tool.

Proven In Use is only required for tools that affect and can change the embedded code or processor.

 

Best regards,

Daniel